Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide5

In addition, as a number of discrete components are involved, varying tolerances and temperature drifts combined with additional noise can further impact system accuracy, especially when working with small signals. Aside from component selection and board space challenges, numerous discrete components can make error budgets difficult to calculate. With this in mind, Analog Devices has developed a new converter architecture to address these issues and provide a unique single chip solution.

PTM Published on: 2007-09-17