Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide16

The Frequency Increment is a 24-bit word that is programmed to the on-board RAM at addresses 85 h, 86 h, and 87 h. The required code loaded to the Frequency Increment register is based on the master clock frequency and the required increment frequency output from the DDS as follows: Frequency Increment code = ( Required frequency increment / (MCLK / 4)) x 227.

PTM Published on: 2007-09-17