Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide22

The above example shows the calculation of an unknown impedance using the previously calculated Gain Factor. It is important to note that because the AD5933 has a finite frequency response, the gain factor also has a variation with frequency resulting in an error in the impedance calculation over a frequency range. To minimize this error, the frequency sweep should be limited to the smallest frequency range as possible (e.g., from 30KHz to 32KHz).

PTM Published on: 2007-09-17