Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
T9602-Slide11

In summary, compared to typical humidity and temperature sensors in the industry the Telaire T9602 saves on the number of components used as it communicates directly with the controller. It is available in analog or digital versions and as clip surface mount or through panel mount. It comes pre-calibrated and with a quick installation is a solution ready to go out of the box.

PTM Published on: 2015-05-18