Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Topic 4 Control Subsystem Slide 16

One of the biggest things is that TI included some additional timer functions in the Concerto devices, primarily timer 2 clocking and control registers. The user can configure CPU timer 2 to be also clocked by an external oscillator or the on-chip 10 MHz oscillator. The user can then use CPU timer 0 or CPU timer 1 to monitor the CPU clock source and use CPU timer 2 to monitor the independent clock source. Additionally, TI has maintained the eCAP, eQEP and an additional COM port, so other than the timer, the external captures and the external COM ports, there has not been any changes here.

PTM Published on: 2012-06-20