Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Topic 4 Control Subsystem Slide 10

The M3 memory information and the control relative memory information is always expressed in bytes. The C28x memory map in the datasheet will likely refer to 16-bit words as well as its link command file. The DMA controller, that can transfer data to and from the on-chip SRAM and some peripherals, can not transfer data from the flash memory or ROM, because the flash memory and ROM are located on a separate internal bus.

PTM Published on: 2012-06-20