Maker.io main logo

Creating Docker Instances

25

2026-05-18 | By Andrew Kazour

Overview

In this post, I will show how I made a static web server using Docker and Docker Compose. All steps documented below allow a peer to recreate the environment from scratch on an Ubuntu virtual machine.

  • I demonstrate how to create 5 containers to which you can connect and have different services running on each of them

Docker is a great way to run services in an isolated manner to allow for security and a good way to test services.

Creating the Ubuntu Instance (AWS)

An Ubuntu Server virtual machine was created using Amazon Web Services (AWS). The instance was configured with the OS only and on Ubuntu 22.04:

Image of Creating Docker Instances

Dual stack is selected with the 90-day free trial hardware selection:

Image of Creating Docker Instances

I am a really big fan of AWS, as it is easy to use, and they give free trials for everything, so you will know if you want to continue using it or not. It’s also relatively low cost, as 5 dollars a month isn't a big expense.

Change Network settings

Go to the Network tab and add a rule to the IPv4 to allow for all TCP traffic. This is so you will be able to connect to your web service and not be blocked by the firewall:

Image of Creating Docker Instances

When I was setting this up, I ended up not changing the TCP settings, which meant I couldn't connect to it since it blocked all connections! After that, I opened all ports, which isn't the most secure, but for this basic use, it is fine.

Docker setup and installation

Docker was installed following the official Docker documentation for Ubuntu to ensure compatibility and stability.

Step 1: Update package index and install prerequisites

Copy Code
sudo apt-get update
sudo apt-get install -y ca-certificates curl

Step 2: Add Docker’s official GPG key

Copy Code
sudo install -m 0755 -d /etc/apt/keyrings
sudo curl -fsSL https://download.docker.com/linux/ubuntu/gpg -o /etc/apt/keyrings/docker.asc
sudo chmod a+r /etc/apt/keyrings/docker.asc

Step 3: Add Docker repository to APT sources

Copy Code
echo \
  "deb [arch=$(dpkg --print-architecture) \
  signed-by=/etc/apt/keyrings/docker.asc] \
  https://download.docker.com/linux/ubuntu \
  $(. /etc/os-release && echo "$VERSION_CODENAME") stable" | \
  sudo tee /etc/apt/sources.list.d/docker.list > /dev/null
 
Copy Code
sudo apt-get update

Step 4: Install Docker Engine and required components

Copy Code
sudo apt-get install -y docker-ce docker-ce-cli containerd.io docker-buildx-plugin docker-compose-plugin

Step 5: Verify Docker installation

Copy Code
sudo docker run hello-world

A successful message confirms Docker was installed correctly, and then you can go on to the final steps.

Step 6: Post Docker steps

To allow Docker commands to be run without sudo, the following steps are performed:

Copy Code
sudo groupadd docker
sudo gpasswd -a $USER docker
newgrp docker

Step 7: Docker Compose steps

Docker Compose needs to be enabled:

Copy Code
sudo curl -L \
"https://github.com/docker/compose/releases/download/1.29.2/docker-compose-$(uname -s)-$(uname -m)" \
-o /usr/local/bin/docker-compose
Copy Code
sudo chmod +x /usr/local/bin/docker-compose

Verification:

Copy Code
docker-compose --version

If this verification step shows a version, then you have completed the setup of Docker!

Docker is best run on Linux, which is why we went through a VM with Ubuntu. I have tried using Docker on Windows, but it just isn’t as good and doesn’t give me the same results.

Nginx Server in a Custom Container

Static Website Preparation

The static website files were organized in a clear directory structure:

  • index.html as the main entry point
  • Additional assets stored in appropriate subdirectories

You can make any website or service you want to run. I just made a quick sample website that allowed me to see that Docker was working.

Docker File creation

A Dockerfile is created in the root directory of the project with this inside it:

Copy Code
FROM nginx:stable-alpine
COPY ./usr/share/nginx/html
EXPOSE 80
CMD ["nginx", "-g", "daemon off;"]

This Dockerfile:

  • Uses a Nginx base image
  • Copies website files into the container
  • Exposes port 80
  • Runs Nginx in the foreground

Build the Container Image

Copy Code
docker build -t my-nginx-container

Verification that it was built properly:

docker image ls

Run this first container

Copy Code
docker run -p 8080:80 my-nginx-container
  • Test it using a web browser
http://your-instance-ip-address:8080

These are the final steps in setting up one container to run whatever you want. Below this, I will show running 5 containers, which could be a better use case for a lot of people.

Replicating 5 Identical Containers

Overview

We have to make a Docker Compose file to run multiple Docker containers at once! The file below shows how I made 5 containers, where they all use the same index.html file. All the containers are on separate ports and can be used for redundancy of a website.

docker-compose.yml (Identical Services)

Copy Code
services:

  web1:

    image: my-nginx-container

    container_name: web1

    ports:

      - "8081:80"

    volumes:

      - ./index.html:/usr/share/nginx/html/index.html:ro




  web2:

    image: my-nginx-container

    container_name: web2

    ports:

      - "8082:80"

    volumes:

      - ./index.html:/usr/share/nginx/html/index.html:ro




  web3:

    image: my-nginx-container

    container_name: web3

    ports:

      - "8083:80"

    volumes:

      - ./index.html:/usr/share/nginx/html/index.html:ro




  web4:

    image: my-nginx-container

    container_name: web4

    ports:

      - "8084:80"

    volumes:

      - ./index.html:/usr/share/nginx/html/index.html:ro




  web5:

    image: my-nginx-container

    container_name: web5

    ports:

      - "8085:80"

    volumes:

      - ./index.html:/usr/share/nginx/html/index.html:ro

Run the Services

Copy Code
docker compose up -d

To close the service, use this:

Copy Code
docker compose down

Verification:

Copy Code
docker compose ps

Each container serves identical content on different ports.

Replicating 5 unique Containers

Overview

We can now edit the Docker compose file to run unique services on each container. This is almost the exact same as the last one, but we have to change the index.html file for each service.

docker-compose-unique.yml (Unique Services)

The creation of the unique service using the same compose file layout, except with a change to the directory structure:

volumes:

- ./index.html:/usr/share/nginx/html/index.html:ro

Change the index.html to a different service for each container (index2.html, Wikipedia.html, etc.). This will map the service you put in the path to the port in that same set.

Run the Services

Copy Code
docker compose -f docker-compose-unique.yml up -d

To close the service, use this:

Copy Code
docker compose -f docker-compose-unique.yml down

Verification:

You can verify it worked by testing with the “curl” command. When you send the command, it will show the HTML code of the specific service you have in that port. Change the ports to whatever ports you used.

Copy Code
curl localhost:8081
curl localhost:8082
curl localhost:8083
curl localhost:8084

Accessing the website

To access the website, you must use the public IPV4 address and the port the website is on. This could look something like:

http:\\52.220.90.31:8080

You can find the public IPV4 address on AWS Lightsail, and then you use the port you put in the Docker Compose files. You will want to make sure you click the button to make it static, so if you restart an Ubuntu instance, you don't have to get a whole new IP to access it. I didn't make it static at first, and it caused me a headache!

Image of Creating Docker Instances

Conclusion of the container creation

Using this setup guide, you will be able to create a Docker and Docker Compose file to create containers for your services. You will be able to create multiple web services based on the number of services you have, as well as ports.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.