Maker.io main logo

The Ultimate Smartphone VFO ESP32 & Si5351 Wireless Control

25

2026-05-11 | By Mirko Pavleski

License: General Public License ESP32

Variable frequency oscillators (VFOs) are commonly used in radio transmitters and receivers, especially superheterodyne receivers, where they allow the adjustment of the operating frequency. They are essential for amateur radio, communication systems, and test electronics. In several of my previous videos, I have shown you several different ways to create VFOs, which basically differ in the way the generated frequency is displayed.

This time, I will again describe a way to make such a device, but now it is significantly different and more practical than the previous ones.

However, its manufacture is much simpler and cheaper, because we do not use a display or even a rotary encoder, which is a basic part of every VFO. All this is achieved thanks to the use of a smartphone in the function of controlling and displaying the generated frequencies. Now the device is extremely simple and consists of only two inexpensive components: an ESP32 microcontroller board and a Si5351 clock generator module, which is connected to the ESP32 with only 4 wires.

yuyu

The frequency is generated directly on the CLK0 output of the signal generator. Using a smartphone as a user interface (UI) instead of a classic LCD is a great way to get a graphically rich display without spending money on expensive touchscreens. The ESP32 is perfect for this because it has built-in Wi-Fi and enough muscle to simultaneously run a web server and communicate with the Si5351 via the I2C protocol.

At first, the challenge was to achieve that "smooth" rotation effect without lag, so I started with the ESPAsyncWebServer library, which allows control via WebSocket, but several bugs appeared, so I continued with the built-in WiFi.h and WebServer.h libraries, which are quite sufficient for optimal control and operation of the device. Then I gradually created a visually beautiful graphical interface with an LCD, a central rotary knob, and more functional small buttons with different functions.

hik

The code is designed in a way that you can easily change multiple parameters, from bandwidth and frequencies to changing all the colors in one place.

First, let me explain to you the method of starting and all the functions of this hybrid VFO. We turn on the hardware part, and on the smartphone we search for a Wi-Fi network (access point) with the name SI5351_VFO_Final_Complete.

yu

Then we connect to that network with the password "vfo12345678". Now, in the web browser, we enter the address 192.168.4.1. By pressing enter, a mask of a professionally made instrument appears on the display. This image actually represents a web interface through which we will control the hardware. A great advantage is the fact that we do not install any applications on the smartphone at all, but only open a web page.

jbkj

Thus, there is no danger of introducing malicious software, and the compatibility with different smartphone models is unlimited, taking into account that the only requirement is to activate a web browser. By pressing the bottom of the display, full-screen mode is activated, and now the instrument is ready for operation. The LCD shows the starting frequency, which is defined in the code. The upper left part of the screen shows the modulation type and the band, and the lower left shows the step with which the frequency changes. At the very bottom right is the Signal Bar, which in a real receiver or transmitter would display the signal strength. This bar is connected to GPIO34, and by applying a voltage signal to this input, the display is activated. Below the display is a large round knob centrally placed with which we set the desired frequency. As I said earlier, the knob moves very smoothly, and the data is transmitted almost instantly to the device. In reality, during operation, there is no noticeable delay at all. Several small functional buttons follow.

- First, the Amateur band areas are defined.

- Below them is the STEP button, which is very often used and, therefore, larger.

- Below STEP are the MODE buttons AM, SSB, USB, FM

- And at the bottom are the memory buttons.

pok

If we want to memorize a frequency, we first press the number at the top of the display, during which the memory buttons start flashing, and by pressing one of them, the frequency is memorized. In case we want to delete all previously memorized frequencies, press the button in the middle of the LCD.

Now let's see how this device works in real conditions.

hj

To do this, we will connect a small oscilloscope to the output of the hardware part, on which we will observe the change in frequency and signal shape.

And finally, a short conclusion. This project proves you don't need expensive touchscreens to have a beautiful, professional-grade interface for your radio projects. By combining an ESP32 and an Si5351 with your smartphone, you can build a highly functional, retro-styled VFO that fits right in your pocket.

m

Copy Code
// by mircemk May, 2026

#include <WiFi.h>
#include <WebServer.h>
#include <si5351.h>
#include <Wire.h>

Si5351 si5351;
unsigned long frequency = 7000000;
const char* ssid = "Si5351_VFO_Final_Complete";
const char* password = "vfo12345678";

WebServer server(80);

const char VFO_HTML[] PROGMEM = R"rawliteral(
<!DOCTYPE html><html><head>
<meta name="viewport" content="width=device-width, initial-scale=1, maximum-scale=1, user-scalable=0">
<style>
  :root { 
    /* ТУКА СЕ МЕНУВААТ БОИТЕ - ВЕРЗИЈА V2.4 */
    --panel-bg: #E0AB07;      
    --inner-bezel:#E0AB07 //#56748F;   
    --lcd-bg: #0077c2;        
    --btn-band: #7f0000;      
    --btn-step: #27ae60;      
    --btn-mode: #2980b9;      
    --btn-mem: #8e44ad;       
    --gold-border: #f1c40f;   
    --text-color: #ecf0f1;    
  }

  * { -webkit-tap-highlight-color: transparent; box-sizing: border-box; -webkit-touch-callout: none; -webkit-user-select: none; user-select: none; }
  body { background: #000; margin: 0; padding: 0; display: flex; justify-content: center; font-family: 'Arial Black', sans-serif; color: var(--text-color); overflow: hidden; }
  .vfo-main-frame { background: var(--panel-bg); width: 100%; max-width: 400px; height: 100vh; display: flex; flex-direction: column; align-items: center; border-left: 2px solid #444; border-right: 2px solid #111; }
  
  .bezel-display { background: var(--inner-bezel); width: 92%; margin-top: 15px; padding: 10px; border-radius: 8px; box-shadow: inset 4px 4px 10px #000, 2px 2px 5px rgba(255,255,255,0.1); position: relative; }
  
  .fs-zone { position: absolute; left: 0; top: 0; width: 30%; height: 100%; z-index: 10; cursor: pointer; }
  .mem-zone { position: absolute; left: 30%; top: 0; width: 40%; height: 100%; z-index: 10; cursor: pointer; }
  .reset-zone { position: absolute; right: 0; top: 0; width: 30%; height: 100%; z-index: 10; cursor: pointer; }

  .display { background: var(--lcd-bg); border: 4px solid #111; padding: 10px; box-shadow: inset 0 0 25px #000; height: 125px; display: flex; flex-direction: column; justify-content: space-between; position: relative; transition: background 0.2s; }
  .display.mem-active { background: #e67e22; }
  .display.reset-flash { background: #e74c3c; }

  .display-info { display: flex; justify-content: space-between; font-size: 14px; color: rgba(255,255,255,0.9); font-family: Arial, sans-serif; }
  #f-display { font-size: 55px; font-weight: 900; margin: 0; text-align: right; text-shadow: 2px 2px 4px #000; letter-spacing: -1px; line-height: 1; }
  
  .display-footer { display: flex; align-items: center; border-top: 1px solid rgba(255,255,255,0.2); padding-top: 5px; margin-bottom: 4px; }
  #mode-label, .sig-text { font-size: 15px; font-weight: bold; }
  
  .s-meter-container { display: flex; align-items: center; gap: 6px; flex-grow: 1; justify-content: flex-end; margin-left: 25px; }
  .s-grid { display: flex; gap: 1px; height: 10px; width: 115px; background: rgba(0,0,0,0.3); border: 1px solid #111; }
  .s-seg { flex: 1; background: #222; }
  .s-on { background: #ffffff; box-shadow: 0 0 6px #ffffff; }

  .bezel-knob { background: var(--inner-bezel); width: 270px; height: 270px; margin: 25px 0; border-radius: 50%; box-shadow: inset 3px 3px 10px #000, 2px 2px 5px rgba(255,255,255,0.05); display: flex; justify-content: center; align-items: center; }
  #knob { width: 240px; height: 240px; background: conic-gradient(from 0deg, #333, #777 25%, #333 50%, #777 75%, #333); border-radius: 50%; border: 12px solid #1a1a1a; position: relative; will-change: transform; cursor: pointer; box-shadow: 5px 10px 20px #000; }
  #knob::after { content: ''; position: absolute; top: 25px; left: 50%; transform: translateX(-50%); width: 24px; height: 24px; background: #111; border-radius: 50%; box-shadow: inset 2px 2px 5px #000; }

  .controls-container { width: 94%; display: flex; flex-direction: column; }
  .grid { display: grid; gap: 6px; width: 100%; grid-template-columns: repeat(4, 1fr); }
  .group-margin { margin-bottom: 12px; }
  
  .btn { border: 3px solid var(--gold-border); border-radius: 8px; color: #fff; font-weight: 900; font-size: 15px; padding: 11px 0; text-align: center; cursor: pointer; box-shadow: 3px 5px 8px #000; text-transform: uppercase; transition: transform 0.05s; }
  .btn:active { transform: translateY(2px); box-shadow: 1px 2px 4px #000; }
  
  .b-band { background: var(--btn-band); }
  .b-step { background: var(--btn-step); font-size: 20px; padding: 12px; grid-column: span 4; }
  .b-mode { background: var(--btn-mode); }
  .b-mem { background: var(--btn-mem); border-color: #555; font-size: 13px; }
  
  .signature { color: #555; font-size: 16px; margin-top: 20px; text-align: center; width: 100%; padding-bottom: 15px; font-weight: normal; }
</style>
</head><body>
  <div class="vfo-main-frame">
    <div class="bezel-display">
      <div class="fs-zone" onclick="toggleFS()"></div>
      <div class="mem-zone" onclick="startMem()"></div>
      <div class="reset-zone" onclick="clearAllMem()"></div>
      
      <div class="display" id="main-display">
        <div class="display-info"><span id="band-label">40M HAM</span><span id="step-label">100Hz</span></div>
        <h1 id="f-display">07.000.000</h1>
        <div class="display-footer">
          <span id="mode-label">USB</span>
          <div class="s-meter-container">
            <span class="sig-text">Sig:</span>
            <div class="s-grid" id="s-grid"></div>
          </div>
        </div>
      </div>
    </div>
    <div class="bezel-knob"><div id="knob"></div></div>
    <div class="controls-container">
      <div class="grid group-margin">
        <div class="btn b-band" onclick="setBand(531000, 'MW')">MW</div>
        <div class="btn b-band" onclick="setBand(1810000, '160M')">160</div>
        <div class="btn b-band" onclick="setBand(3500000, '80M')">80</div>
        <div class="btn b-band" onclick="setBand(7000000, '40M')">40</div>
        <div class="btn b-band" onclick="setBand(14000000, '20M')">20</div>
        <div class="btn b-band" onclick="setBand(18068000, '17M')">17</div>
        <div class="btn b-band" onclick="setBand(21000000, '15M')">15</div>
        <div class="btn b-band" onclick="setBand(24890000, '12M')">12</div>
      </div>
      <div class="grid group-margin">
        <div class="btn b-step" id="step-btn" onclick="nextStep()">STEP: 100Hz</div>
      </div>
      <div class="grid">
        <div class="btn b-mode" onclick="setMode('AM')">AM</div>
        <div class="btn b-mode" onclick="setMode('USB')">USB</div>
        <div class="btn b-mode" onclick="setMode('LSB')">LSB</div>
        <div class="btn b-mode" onclick="setMode('FM')">FM</div>
        <div class="btn b-mem" id="m1" onclick="handleMem(1)">M1</div>
        <div class="btn b-mem" id="m2" onclick="handleMem(2)">M2</div>
        <div class="btn b-mem" id="m3" onclick="handleMem(3)">M3</div>
        <div class="btn b-mem" id="m4" onclick="handleMem(4)">M4</div>
      </div>
    </div>
    <div class="signature">Si5351 VFO by mircemk</div>
  </div>

  <script>
    var freq = 7000000;
    var curMode = "USB"; var lastAngle = 0; var curRot = 0; var isDrag = false; var lastSent = 0;
    var steps = [10, 100, 1000, 5000, 10000, 100000];
    var stepLabels = ["10Hz", "100Hz", "1KHz", "5KHz", "10KHz", "100KHz"];
    var stepIdx = 1;
    var isMemMode = false;

    function loadSavedMem() {
      for(let i=1; i<=4; i++){
        let saved = localStorage.getItem('vfo_m'+i);
        if(saved) document.getElementById('m'+i).innerText = (saved/1000000).toFixed(3);
        else document.getElementById('m'+i).innerText = "M"+i;
      }
    }

    function clearAllMem() {
      for(let i=1; i<=4; i++) localStorage.removeItem('vfo_m'+i);
      loadSavedMem();
      let d = document.getElementById('main-display');
      d.classList.add('reset-flash');
      setTimeout(() => d.classList.remove('reset-flash'), 300);
    }

    function startMem() {
      isMemMode = true;
      document.getElementById('main-display').classList.add('mem-active');
      document.querySelectorAll('.b-mem').forEach(b => b.classList.add('save-ready'));
    }

    function handleMem(id) {
      if(isMemMode) {
        localStorage.setItem('vfo_m'+id, freq);
        document.getElementById('m'+id).innerText = (freq/1000000).toFixed(3);
        isMemMode = false;
        document.getElementById('main-display').classList.remove('mem-active');
        document.querySelectorAll('.b-mem').forEach(b => b.classList.remove('save-ready'));
      } else {
        let saved = localStorage.getItem('vfo_m'+id);
        if(saved) { freq = parseInt(saved); updateUI(); sendFreq(); }
      }
    }

    function toggleFS() {
      var d = document.documentElement;
      if(!document.fullscreenElement) d.requestFullscreen().catch(e=>{});
      else document.exitFullscreen();
    }

    function updateBandLabel() {
      let b = document.getElementById('band-label');
      // ПРЕЗЕМЕНИ ОПСЕЗИ ОД V1.9
      if (freq >= 1810000 && freq <= 2000000) b.innerText = "160M HAM";
      else if (freq >= 3500000 && freq <= 3800000) b.innerText = "80M HAM";
      else if (freq >= 7000000 && freq <= 7200000) b.innerText = "40M HAM";
      else if (freq >= 14000000 && freq <= 14350000) b.innerText = "20M HAM";
      else if (freq >= 18068000 && freq <= 18168000) b.innerText = "17M HAM";
      else if (freq >= 21000000 && freq <= 21450000) b.innerText = "15M HAM";
      else if (freq >= 24890000 && freq <= 24990000) b.innerText = "12M HAM";
      else if (freq >= 28000000 && freq <= 29700000) b.innerText = "10M HAM";
      else if (freq >= 531000 && freq <= 1602000) b.innerText = "MW BROADCAST";
      else if (freq >= 5900000 && freq <= 6200000) b.innerText = "49M BROADCAST";
      else if (freq >= 7200001 && freq <= 7450000) b.innerText = "41M BROADCAST";
      else if (freq >= 9400000 && freq <= 9900000) b.innerText = "31M BROADCAST";
      else if (freq >= 11600000 && freq <= 12100000) b.innerText = "25M BROADCAST";
      else if (freq >= 15100000 && freq <= 15830000) b.innerText = "19M BROADCAST";
      else b.innerText = "GEN";
    }

    function updateUI() {
      document.getElementById('f-display').innerText = Number(freq).toLocaleString('de-DE').replace(/,/g, '.');
      document.getElementById('mode-label').innerText = curMode;
      updateBandLabel();
    }

    function setBand(f, n) { freq = f; updateUI(); sendFreq(); }
    function setMode(m) { curMode = m; updateUI(); }
    function nextStep() {
      stepIdx = (stepIdx + 1) % steps.length;
      document.getElementById('step-btn').innerText = "STEP: " + stepLabels[stepIdx];
      document.getElementById('step-label').innerText = stepLabels[stepIdx];
    }
    function sendFreq() {
      let now = Date.now();
      if (now - lastSent > 50) { fetch('/set?f=' + freq); lastSent = now; }
    }
    function getAngle(x, y) {
      let r = document.getElementById('knob').getBoundingClientRect();
      return Math.atan2(y - (r.top + r.height/2), x - (r.left + r.width/2)) * 180 / Math.PI;
    }
    function move(e) {
      if (!isDrag) return;
      let ev = e.touches ? e.touches[0] : e;
      let ang = getAngle(ev.clientX, ev.clientY);
      let d = ang - lastAngle;
      if (d > 180) d -= 360; if (d < -180) d += 360;
      curRot += d;
      freq += Math.round(d) * (steps[stepIdx] / 10);
      if (freq < 100000) freq = 100000;
      updateUI();
      document.getElementById('knob').style.transform = 'rotate(' + curRot + 'deg)';
      sendFreq();
      lastAngle = ang;
    }
    let knob = document.getElementById('knob');
    knob.addEventListener('mousedown', function(e) { isDrag = true; lastAngle = getAngle(e.clientX, e.clientY); });
    knob.addEventListener('touchstart', function(e) { isDrag = true; lastAngle = getAngle(e.touches[0].clientX, e.touches[0].clientY); e.preventDefault(); }, {passive: false});
    window.addEventListener('mouseup', () => isDrag = false);
    window.addEventListener('touchend', () => isDrag = false);
    window.addEventListener('mousemove', move);
    window.addEventListener('touchmove', move, {passive: false});
    
    setInterval(() => {
      fetch('/getS').then(r => r.text()).then(v => {
        let segs = document.querySelectorAll('.s-seg');
        let act = Math.floor((v/100)*20);
        segs.forEach((s,i) => { if(i<act) s.classList.add('s-on'); else s.classList.remove('s-on'); });
      });
    }, 250);

    loadSavedMem();
    updateUI();
  </script>
</body></html>
)rawliteral";

void updateFrequency(unsigned long f) { si5351.set_freq(f * 100ULL, SI5351_CLK0); }

void setup() {
  Serial.begin(115200); Wire.begin(21, 22);
  pinMode(32, INPUT); 
  analogReadResolution(12); 
  analogSetAttenuation(ADC_6db); 
  WiFi.mode(WIFI_AP); WiFi.softAP(ssid, password);
  si5351.init(SI5351_CRYSTAL_LOAD_8PF, 0, 0);
  updateFrequency(frequency);
  server.on("/", []() { server.send(200, "text/html", VFO_HTML); });
  server.on("/set", []() { if (server.hasArg("f")) { frequency = server.arg("f").toInt(); si5351.set_freq(frequency * 100ULL, SI5351_CLK0); server.send(200, "text/plain", "OK"); } });
  server.on("/getS", []() { int val = analogRead(32); int percent = map(val, 0, 1200, 0, 100); if(percent > 100) percent = 100; server.send(200, "text/plain", String(percent)); });
  server.begin();
}
void loop() { server.handleClient(); }
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.