Maker.io main logo

The Beginners Guide To The New micro:bit Python Editor

27

2023-03-02 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Guide by Kitronik Maker

The 3rd of October saw the release of the new micro:bit Python ‎Editor by the micro:bit Educational Foundation. This guide has been produced to ‎help you get going straight away. This guide also contains a video that walks you ‎through the basics, essential viewing for the new user.‎‎ ‎

What is Python?

Python is a computer programming language that was first released in 1991. It was ‎designed to be fun and easy to learn and to be a multi-purpose language. ‎Today, Python is the most widely used and fastest growing developer language in ‎the world and has a broad application of uses. From powering machine learning to ‎web development and data analytics. From a developer’s point of view, ‎development with Python is often very fast, as Python does not need to be ‎compiled.‎

"Python is fast enough for our site and allows us to produce ‎maintainable features in record times, with a minimum of ‎developers," said Cuong Do, Software Architect, YouTube.com. ‎

Despite being easier to learn than most other text-based languages, it can still be ‎difficult in the early stages of learning. This also makes it challenging for teachers, ‎who have to devise ways in which to help students overcome those initial hurdles. ‎This was one of the main drivers for the development of the new micro:bit Python ‎editor.‎

Video Guide:‎

 

Watch the video for look at how to use the micro:bit Python editor. If you have a ‎little more time on your hands and want to have a go at some tasks, you can also ‎read through the text guide below, which contains a little extra information.‎‎ ‎

The Beginners Guide To The New micro:bit Python Editor:

‎The new editor has lots of features designed to make it easier to teach and learn ‎Python, It removes all of the usual hurdles that make learning text based ‎languages tricky for the beginner. It does this by providing easy to find snippets of ‎code that you can quickly drag and drop into the editor. All of the code contained in ‎the snippet is full visible and fully editable, making it easy to shape the code to ‎your needs. In the next section we'll take a closer look at the editor.‎

‎OPEN THE PYTHON EDITOR!‎‎ ‎

The Editor:

editor_1

We have highlighted four areas of the editor in the above image; 1 - Code Library, ‎‎2 - The workspace, 3 - The micro:bit simulator, 4 - Send code to the micro:bit. ‎

First, we will explore what these 4 areas are and how to use them. After that we'll ‎construct a simple program, and then run it using the simulator.‎

SECTION 1 - CODE LIBRARY:‎

This section contains the reference section which contains all of the available code ‎snippets. Today's guide will focus solely on the Reference menu, as this is where ‎the general code snippets are.‎

library_2 ‎ ‎

Select one of the menu items, such as Display and a list of all of the available code ‎snippets for that section will be displayed. You can then simply click on one of the ‎snippets of code and drag it into the workspace (Section 2), as shown above. This ‎code will display a heart image on the micro:bits LED matrix display. ‎

Activity: Have a browse through the snippet headings, (Variables, Display, ‎Buttons etc) to get a feel for how the snippets have been organised.‎

SECTION 2 - THE WORKSPACE:

Section 2 is the coding workspace; this is where you build you programs. Initially ‎you will drag almost all of the code over from the Reference section and edit it to ‎suit. The editor isn't all about drag and drop, it is also built to allow you to grow as ‎a coder and to offer you new assisting features as you do.‎

workspace_3

As you gain understanding and confidence, more and more of the code in the ‎workspace will be typed directly into the editor. As you type, the editor will assist ‎you with suggestions that you can navigate with the arrow keys and then select. ‎This helps to protect your code from typos, and once you've become accustomed ‎to selecting them, will speed things up nicely. ‎

Activity: Try typing random words into the editor to see what the suggestions pop ‎up looks like. Try using the arrow keys to move up and down the list and then ‎select one of the suggestions. You will soon come to realise how useful these ‎features are. ‎

SECTION 3 - THE SIMULATOR:‎

Section 3 of the editor is the micro:bit simulator, this is a great tool for both testing ‎your software in place and it also allows someone who doesn't have a physical ‎micro:bit to run their code once it is complete. ‎

simulator_4

As you build your code, the simulated micro:bit will be grayed out and there will be ‎a large play icon over it. Once your program is ready to be run/tested, just click on ‎the play icon and your code will run on the simulator in just the same way as it ‎would on an actual micro:bit. ‎

Underneath the editor you will notice a variety of sliders and buttons. These cover ‎a number of functions, buttons, the logo, shake. As the simulated micro:bit is static ‎some of the buttons allow you to test movement based functions. The sliders allow ‎you to test code for things such as sound, temperature, compass heading etc.‎

Activity: Try clicking on some of the buttons underneath the editor, like A, B, and ‎logo and see what happens. Hint, this will only work if the micro:bit is not ‎grayed out. Try running a simple snippet first.‎

SECTION 4 - SENDING A PROGRAM TO A CONNECTED MICRO:BIT:‎

Once you've completed your program and tested your program, the next step is to ‎download the code directly to your micro:bit. It's as simple as clicking the Send to ‎micro:bit button and following a couple of onscreen instructions. Firstly you will be ‎asked to connect the micro:bit to your computer via USB, then you will be ‎asked to choose the micro:bit and press the select button.

sending_5

It's that simple! Now that we've had a look at the basics of using the editor, it's time ‎to try our hand and making something simple and getting it to run on the simulator. ‎

Let's Code - Activity:‎

Browse the Reference menus and look in Display. Before dragging and dropping ‎the code snippet at the top that displays a heart, try changing the heart to another ‎image first. Once you've chosen your image, drag and drop the code snippet into ‎the workspace.‎

activity_6

Now the code has been built, all that remains is to run it. Press the large play icon ‎on the simulator and watch the image that you chose appear on the simulated LED ‎matrix! For extra bonus points, if you have a micro:bit and a USB cable to hand, ‎why not download your code onto the micro:bit and test it there too.‎‎ ‎

TRY THE PYTHON EDITOR!‎‎

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.