Maker.io main logo

NEMA 17 Stepper Motor - Using Encoder for Controlling Speed & Direction

31

2026-06-08 | By Ron Cutts

License: GNU Lesser General Public License I2C / TWI Microcontrollers Serial / UART Arduino ESP32

In this tutorial, we will learn how to use an encoder to control the speed and direction of the NEMA 17 stepper motor using Arduino.

Watch the video!

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

What You Will Need photo 9

The Circuit

  • Arduino Digital Pin 2 will be used for the steps

  • Arduino Digital Pin 3 will be used for motor direction.

If using a Stepper Motor Driver Shield:

  • Connect the Motor Shield GND pin to the Arduino negative pin [GND]

  • Connect the Motor Shield [5V] pin to the Arduino positive pin [5V]

  • Connect the Motor Shield GND pin to the Power Supply negative pin [GND]

  • Connect Motor Shield [9V] pin to Power Supply positive pin [+]

  • Connect the Motor Shield pin[S] to the Arduino digital pin [2]

  • Connect the Motor Shield pin[D] to the Arduino digital pin [3]

  • Connect the stepper motor as shown in the picture.

If using a Stepper Motor Driver 8825:

  • Connect the DRV8825 GND pin to the Arduino negative pin [GND]

  • Connect the DRV8825 DIR pin to Arduino digital pin [3]

  • Connect the DRV8825 STEP pin to Arduino digital pin [2]

  • Connect the Power Supply for the motor to the DRV8825 VMOT and GND

  • Connect the Capacitor across VMOT and GND

  • Connect the stepper motor as shown in the picture.

Connecting the Encoder module:

  • Connect the Encoder module pin [CLK] to Arduino digital pin [5]

  • Connect the Encoder module pin [DT] to Arduino digital pin [6]

  • Connect the Encoder module pin [SW] to Arduino digital pin [7]

The Circuit

The Circuit photo 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  • Add "Multiply Integer By Value" component

  • Add "Rotary Encoder Sensor" component

  • Add "Pulse Generator" component

  • Add "Toggle(T) Flip-Flop" component

  • Add "Debounce Button" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Add Components photo 5

In Visuino Set Components

  • Select "MultiplyByValue1" and in the Properties window set "Value" to 50

  • Select "PulseGenerator1" and in the properties window set "Frequency" to 2000 << this will be the default starting speed of the stepper motor, you can adjust it to your needs

  • select "Frequency" and click on the Pin icon and select "Float SinkPin"

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Connect Components

  • Connect Arduino digital pin [6] to "RotaryEncoderSensor1" pin [Direction]

  • Connect Arduino digital pin [5] to "RotaryEncoderSensor1" pin [Clock]

  • Connect "RotaryEncoderSensor1" pin [Out] to "MultiplyByValue1" pin [In]

  • Connect "MultiplyByValue1" pin [Out] to "PulseGenerator1" pin [In]

  • Connect "PulseGenerator1" pin [Out] to "TFlipFlop1" pin [Clock]

  • Connect "TFlipFlop1" pin [Out] to Arduino digital pin [2]

  • Connect "Button1" pin [Out] to "TFlipFlop2" pin [Clock]

  • Connect "TFlipFlop2" pin [Out] to Arduino digital pin [3]

In Visuino Connect Components

In Visuino Connect Components photo 2

In Visuino Connect Components photo 3

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino module, the motor will start to run, and if you rotate the encoder module, the speed of the motor will change, and if you press a button on the encoder module, the motor will change direction.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.