Digi-Key Electronics to Distribute Mag Layers USA MMD Series Through the Digi-Key Marketplace

Thief River Falls, Minnesota, United States - November 17, 2020

Image of DigiKey to Distribute Mag Layers USA MMD Series Through the DigiKey Marketplace

Digi-Key Electronics, which offers the world's largest selection of electronic components in stock for immediate shipment, announced that it has expanded its product portfolio to include a global distribution of Mag Layers USA MMD series molded power inductors. This partnership is part of Digi-Key's global Marketplace initiative to broaden the product offering now available for customers, making Digi-Key more of a one-stop-shop than ever before.

Mag Layers USA's molded power inductors have a magnetic metal powder core and internal wire coil in a shielded construction for today’s DC/DC applications and power supplies. The MMD series of inductors are produced on state-of-the-art manufacturing lines utilizing second generation automotive grade robotics. These shielded power inductors feature soft saturating core materials in consumer, industrial and automotive grades.

"We are pleased to include Mag Layers USA in our Marketplace solution," said David Stein, vice president of global supplier management for Digi-Key. "Mag Layers USA's offerings for a variety of consumer, industrial and automotive grade clients further round out our power inductor offerings and feature many high levels of compliance that our customers are looking for, from no conflict minerals to Reach and RoHS compliance."

The typical applications for the MMD Series include laptop, desktop and server power, as well as high current power supplies, battery powered devices, and PMIC applications. The MMD series are RoHS/Reach compliant, halogen free, low resistance and offer high current ratings. Mag Layers USA offers sizes from 4 mm x 4 mm to 17 mm x 17 mm.

For more information about Mag Layers USA and to order from their product portfolio, please visit the Digi-Key website.

About Mag Layers USA

Mag Layers USA Inc. was established in 1990 and set out to provide high quality and cost-effective component solutions for a growing electronics industry. In 1997, Mag Layers became the first Taiwanese company in the same industry to receive to ISO9001 certification, in addition they have received QS9000, ISO14001 and TS16949. Mag Layers' remains committed to innovative technology with advanced materials, designs, processing, and automation, helping them develop leading-edge products and bring them to the global market.

About DigiKey

DigiKey, headquartered in Thief River Falls, Minn., USA, is an authorized global, full-service distributor of electronic components, offering more than 10.1 million products from over 1900 quality name-brand manufacturers. DigiKey also offers a wide variety of online resources such as EDA and design tools, datasheets, reference designs, instructional articles and videos, multimedia libraries, and much more. Technical support is available 24/7 via email, phone and webchat. Additional information and access to DigiKey's broad product offering can be found by visiting www.digikey.com.au and on Facebook, Twitter, YouTube, Instagram, and LinkedIn.