Digi-Key Corporation Announces Stock for Weidmuller's New DRAC Line
THIEF RIVER FALLS, Minnesota, USA - November 19, 2009
Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced it has stock for Weidmuller's new line of AC DIN rail receptacles.
The following DRAC line products are now available for purchase on Digi-Key's global websites and will be featured in future print and online catalogs:
- 6720005420 (Digi-Key # 281-2579-ND) Module Outlet AC Dual 20A 120VAC
- 6720005421 (Digi-Key # 281-2580-ND) Module Outlet AC Dual 15A 120VAC
- 6720005422 (Digi-Key # 281-2581-ND) Module Outlet AC GFI 15A 120VAC
- 6720005423 (Digi-Key # 281-2582-ND) Module Outlet AC GFI 20A 120VAC
Compact at only 2.9-inches wide and 4.6-inches wide, these new receptacles are fully enclosed and touch safe. They include 15A or 20A power outlets, which provide a simple and convenient power source inside a panel or closure for such applications as laptops, test equipment, lighting, and solder irons.
The DRAC line offers design flexibility and savings on setup time. Ready to be put into place right out of the box, these receptacles can be installed onto 35mm DIN rail or, for added convenience, directly panel mounted. They accept solid or stranded wiring from 20AWG to 10AWG. Additionally, the DRAC line is UL approved for use in any UL panel or control system. THE UL508A and cULus approvals coupled with NEMA ratings make it effortless to add to a control cabinet or system.
About Weidmuller
Weidmuller is a leading provider of solutions for the transmission of power, data, and control signals in industrial environments. The company develops, produces, and sells industrial electronics, network infrastructure components, and connectivity solutions such as industrial Ethernet, relays, power supplies, I/O modules, printed circuit board connectors, terminal blocks, and complete DIN rail assemblies. The Weidmuller group has a strong international focus with manufacturing and sales locations in over 70 countries. For more information, visit www.weidmuller.com.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com