The OSM Standard for System on Modules Explained
2022-06-23
System on module standards
Various system on module standards, such as SMARC and Qseven (Figure 1), have been adopted by product designers, solution architects and system engineers. SGeT (Standardization Group for Embedded Technologies), an international not-for-profit association of companies and organizations, collaborates and develops independent specifications for embedded computer technology. Choosing an industry standard for system on modules helps in technology scalability and leverages inter-operability amongst suppliers.
Recently, a new standard for system on modules has been defined by SGeT – OSM or open standard module, with the unique value proposition of being a solderable system on module. The standard enables an added layer of ruggedness with the LGA design and surface mount technology.
Figure 1: System on module standards include SMARC, Qseven, and OSM. (Image source: iWave)
OSM standard explained
open standard module, the latest industry standard for system on modules, was launched in December 2020. To create a new, future proof and versatile standard for small size, low-cost embedded computer modules, SGeT released the OSM 1.0 specification. OSM is one of the first standards for directly solderable and scalable embedded computer modules.
OSM is making its way into the industry with postage stamp-sized embedded computer modules by replacing credit card-sized modules. The OSM allows developing, producing and distributing embedded modules for the MCU32, Arm® and x86 architectures. The key characteristics of the OSM module include:
- Completely machine processible during soldering, assembly and testing
- Pre-tinned LGA package for direct soldering without connector
- Pre-defined soft and hard interfaces
- Open-source in software and hardware
The all-new standard is available in four different sizes, ranging across size zero, small, medium, and large, varying on the LGA contacts available on the module (Figures 2a and 2b). The four different form factors can build upon each other.
Figure 2a: Standard OSM sizes, form factors, and pinouts. (Image source: iWave)
Figure 2b: Standard OSM sizes color-coded according to Figure 2a. (Image source: iWave)
The open standard module uses a symmetric LGA package for connecting the module PCB to the baseboard PCB. Fused Tin Gird Array, ENIG LGA or BGA, can be used as the contact technologies, at the discretion of the manufacturer. The specifications also allow for module vendors to adopt different heights based on the requirements, with the option to extend through a “PCB Spacer”.
Modules from size-S upwards offer video interfaces for up to 1x RGB and 4-channel DSI. Size-M modules can additionally support 2x eDP/eDP++, and size-L adds 2x LVDS interface for graphics. Hence maximum configurations can provide up to six video outputs in parallel. All modules from size-S upwards further offer a 4-channel camera serial interface (CSI). Size-L modules provide up to 10 PCIe lanes for quick connection of peripherals; size-M offers 2x PCIe x1, and size-S 1x PCIe x1. In view of the extremely miniaturized footprint, size-0 modules do not feature any of the I/Os mentioned but do offer all the interfaces listed in the OSM specification, which provisions up to 5x Ethernet for system-to-system communication.
In all the modules, there is a dedicated communication area, which provides 18 pins for antenna signals for different wireless technologies, and 19 pins available for manufacturer-specific signals.
Why consider OSM?
The main advantages of the OSM module include PCB solderable module with resistance to vibration, compact form factor with smallest pin-to-area ratio and provision for technology scalability.
Since the module can be directly soldered on the carrier card, the module is a right fit for products which are prone to vibrations and require a compact form factor. An example includes the connectivity cluster for an electric 2-wheeler. OSM Modules provide designers a solution with an ideal mix of scalability, form-factor and cost.
For a growing number of IoT applications, this standard helps to combine the advantages of modular embedded computing with increasing requirements regarding costs, space and interfaces. The potential applications of an OSM module include IoT-connected embedded, IoT, and edge systems that run open-source operating systems and are used in harsh industrial environments.
iWave portfolio of OSM system on modules
iWave Systems, a leader in design and manufacturing of system on modules, recently launched iW-RainboW-G40M (Figure 3): The solderable i.MX 8M Plus OSM Module. iW-Rainbow-G40M integrates the powerful i.MX 8M Plus processor in the compact OSM 1.0 standard, delivering powerful AI and Machine learning capabilities on a compact module.
Figure 3: The top and bottom of the iW-G40M system on module. (Image source: iWave)
Two image signal processors (ISP’s) and a dedicated neural network processor at up to 2.3 TOPS make the i.MX 8M Plus an ideal fit in Smart Home, Smart City, Industrial IoT and beyond with its Machine learning, vision, and advanced multimedia capability.
Key features of the module
- i.MX 8M Plus dual/quad lite/quad
- 2 GB LPDDR4 (up to 8 GB)
- 16 GB eMMC (up to 256 GB)
- Wi-Fi (802.11b/g/n/ac/ax) (ax is optional)
- Bluetooth 5.0
- 2 x CAN-FD ports
- 2 x RGMII interfaces
- PCIe 3.0 x 1
- LVDS x 2
- Size-L LGA module
The module provides designers a flexible and scalable option for their product while shortening their up time to market. With the provision for industrial interfaces such as CAN-FD, time-sensitive networking, and high-speed interfaces, the processor is an ideal fit for Industry 4.0 and automation systems supporting intelligent and fast processing of multi-media data.
Through a development kit and a production-ready SOM, a designer can accelerate time to market with reduced risk. The module is application-ready and comes with all the necessary software drivers and BSPs with software support of Ubuntu, Android and Linux.
Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.