ESP8266 Quick Start Guide Datasheet by Espressif Systems
View All Related Products | Download PDF Datasheet
!
Version 1.4
Copyright © 2017
ESP8266
Quick Start Guide

About This Guide
This document is a quick start guide to ESP8266. The document is structured as follows.
Release Notes
Chapter
Title
Content
Chapter 1
Configuring the Development
Board ESP-LAUNCHER
Introduction to the ESP8266 development board ESP-
LAUNCHER, and how to download firmware to the board and
run it.
Chapter 2
Compiling
ESP8266_NONOS_SDK
Compiling the ESP8266_NONOS_SDK in the virtual machine.
Chapter 3
Compiling
ESP8266_RTOS_SDK
Compiling the ESP8266_RTOS_SDK.
Chapter 4
Common Debug Methods
Common debugging methods and sample codes.
Chapter 5
Downloading Firmware into
the ESP-WROOM-02
Instructions on how to download firmware with ESP-
WROOM-02.
Appendix A
Learning Resources
ESP8266-related must-read documents and must-have
resources.
Date
Version
Release notes
2016.08
V1.0
First release.
2016.11
V1.1
Added Appendix A—Learning Resources.
2017.01
V1.2
Added two Github links to RTOS and non-OS SDK sample
code in Appendix A.2—Must-Have Resources.
2017.02
V1.3
Updated the link to the OVA image file in Section 2.1.
2017.05
V1.4
Updated Chapter 1.

Table of Contents
1. Configuring the Development Board ESP-LAUNCHER 1 .......................................................
1.1. Hardware Preparation!1"................................................................................................................
1.2. Software Preparation!1".................................................................................................................
1.3. Downloading Firmware into the ESP-LAUNCHER!2".....................................................................
2. Compiling ESP8266_NONOS_SDK 7 .......................................................................................
2.1. Downloading the Virtual Machine!7"..............................................................................................
2.2. Setting up Development Environment!7".......................................................................................
2.3. Compiling Process!9".....................................................................................................................
3. Compiling ESP8266_RTOS_SDK 12 ........................................................................................
3.1. Compiling Process!12"...................................................................................................................
3.2. ESP8266_RTOS_SDK Architecture!15"..........................................................................................
4. Common Debug Methods 16 ...................................................................................................
4.1. Common Debug Methods!16"........................................................................................................
4.1.1. Add UART Output Logs!16"..............................................................................................
4.1.2. Debug Fatal Exception!16"...............................................................................................
5. Downloading Firmware into the ESP-WROOM-02 17 .............................................................
A. Appendix—Learning Resources 19 .........................................................................................
A.1. Must-Read Documents!19"............................................................................................................
A.2. Must-Have Resources!20..............................................................................................................

!
1. Configuring the Development Board ESP-LAUNCHER
1. Configuring the Development
Board ESP-LAUNCHER
1.1. Hardware Preparation
To start developing applications for the ESP8266, users need the following hardware and
its corresponding software tools:
•One of the ESP8266 Hardware Development Kits (HDKs) specified below:
- ESP8266’s development board, ESP-LAUNCHER, as shown in Table 1-1.
- ESP8266’s module, ESP-WROOM-02, as described in Chapter 5.
•PC for programming: Windows XP or Windows 7 OS is recommended, with enough
RAM to run a Linux virtual machine.
•Micro-USB cable.
1.2. Software Preparation
•ESP8266’s Flash Download Tool
- Download it from: ESP8266 Flash Download Tools
•ESP8266’s SDK
- Download the SDK from: ESP8266 SDK
📖 Notes:
•When users deploy third-party development boards or modules that integrate ESP8266, they should
use development firmware provided by the corresponding manufacturers.
•To purchase ESP-WROOM-02 or ESP-LAUNCHER, please visit Espressif’s official online store at:
https://espressif.taobao.com,
Table 1-1. The ESP-LAUNCHER
•1 ESP-LAUNCHER
•1 Micro-USB cable
⚠ Notice:
The ESP8266 Wi-Fi module requires 3.3V power supply capable of delivering a peak current of 500 mA.
! !
Espressif
!/211
2017.05

!
1. Configuring the Development Board ESP-LAUNCHER
- The official AT firmware (ESP8266_NONOS_SDK\bin\at) can be downloaded into
the ESP-LAUNCHER by referring to the BIN locations included in the Readme file
which is in the same directory. For instructions on downloading the firmware into ESP-
LAUNCHER, please refer to Section 1.3.
•UART terminal emulator tool
The default baud rate of ESP8266 is74880, therefore, UART tools that can support the
default baud rate are recommended. Please note that certain USB-UART converters
may not support all baud rates if users use a third-party development board.
1.3. Downloading Firmware into the ESP-LAUNCHER
1. We use the ESP8266_NONOS_SDK_V2.0.0_16_07_19 as an example. The AT
firmware binaries are located in
ESP8266_NONOS_SDK_V2.0.0_16_07_19\ESP8266_NONOS_SDK\bin.
!
Figure 1-1. ESP8266_NONOS_SDK BIN Folder
2. Settings of the development board, ESP-LAUNCHER.
!
Figure 1-2. The ESP-LAUNCHER
•switch 1: toggle to the lower side;
Espressif
!/212
2017.05

!
1. Configuring the Development Board ESP-LAUNCHER
•switch 2: toggle to the lower side;
•switch 3: toggle to the upper side;
•pin4: put a jumper cap on the two pins above;
•pin5: put a jumper cap on it.
3. Use a Micro-USB cable to connect ESP-LAUNCHER to the PC. The UART driver needs
to be installed on the PC.
4. Double-click on ESPFlashDownloadTool_v3.3.4.exe to run the ESP8266 Flash
Download Tool on the PC.
!
Figure 1-3. ESP8266 Flash Download Tool
Figure 1-3 uses 16Mbit-C1 (1024+1024 map) flash as an example. The download
addresses are shown in Table 1-2.
Espressif
!/213
2017.05

!
1. Configuring the Development Board ESP-LAUNCHER
5. Click the START button and wait for the ESP-LAUNCHER to power up.
6. Power on the ESP-LAUNCHER by toggling switch 1 as is shown in Figure 1-2 to the
upper side. Toggle switch 2 as is shown in Figure 1-2 to the lower side to enter the
download mode.
7. The ESP8266 Flash Download Tool will start to download AT firmware into the ESP-
LAUNCHER. The DETECTED INFO area will display the information of the flash chip on
ESP-LAUNCHER.
Table 1-2. Download AT Binaries for 16 Mbit-C1 Flash Map
BIN
Address
Description
blank.bin
0x1FB000
It initializes the RF_CAL parameter area.
esp_init_data_default.bin
0x1FC000
It stores the default RF parameter values and has to be
downloaded into the flash at least once.
If the RF_CAL parameter area is initialized, this BIN has to be
downloaded too.
blank.bin
0xFE000
It initializes the user parameter area.
blank.bin
0x1FE000
It initializes the system parameter area.
boot.bin
0x00000
It is the main program located in \bin\at.
user1.2048.new.5.bin
0x01000
It is the main program located in \bin\at\1024+1024.
📖 Note:
The SpiFlashConfig and the COM on the ESP8266 Flash Download Tool should be set according to the
actual situation.
Espressif
!/214
2017.05

!
1. Configuring the Development Board ESP-LAUNCHER
!
Figure 1-4. ESP8266 Flash Download Tool - Downloading Firmware
8. After the download is finished, as Figure 1-5 shows, toggle switch 1 to the lower side to
power off the ESP-LAUNCHER.
!
Figure 1-5. ESP8266 Flash Download Tool–Finishing Downloading Firmware
9. Open the UART tool on the PC, set the baud rate to 115200, and configure new line
mode.
10.Set the ESP8266 to working mode by toggling switch 2 to the upper side. Then toggle
switch 1 to the upper side to power on the ESP-LAUNCHER.
📖 Note:
When using AT commands, then a baud rate of 115200 and new line mode are needed.
Espressif
!/215
2017.05

!
1. Configuring the Development Board ESP-LAUNCHER
The log print may look garbled, as shown in Figure 1-6 (which is normal, because the
default power-on baud rate of ESP8266 is 74880). The “ready” message indicates that
ESP-LAUNCHER is working successfully.
11.Input command AT+GMR and press Enter button. The information of the AT firmware will
appear, as Figure 1-7 shows.
!
Figure 1-6. AT Logs on the UART Tool
For more AT commands and examples, please refer to documents:"
ESP8266 AT Instruction Set and ESP8266 AT Command Examples.!
Espressif
!/216
2017.05

!
2. Compiling ESP8266_NONOS_SDK
2. Compiling
ESP8266_NONOS_SDK
This chapter describes how to compile ESP8266_NONOS_SDK by using the AT demo as
an example.
2.1. Downloading the Virtual Machine
1. PC: Windows XP or Windows 7 OS is recommended.
2. The development environment provided by Espressif Systems is based on Lubuntu. We
also provide a virtual image of the development environment that can be run on
VirtualBox.
•Download VirtualBox-5.0.16-105871-Win.exe from:
https://www.virtualbox.org/wiki/Downloads
•Download ESP8266_lubuntu_20141021.ova from:
http://downloads.espressif.com/FB/ESP8266_GCC.zip
2.2. Setting up Development Environment
Steps
Results
1. Start Windows OS and install the virtual machine.
•Double-click on
VirtualBox-5.0.16-105871-Win.exe
and install VirtualBox.
📖 Note:
VirtualBox has different versions. We are
using Windows V.5.0.16 as an
example.
•Double-click on Oracle VM
VirtualBox.exe to run the program
and the system will display the main
menu 👉.
💬Tip:
ESP8266’s virtual machine takes up
much space (RAM). Please make sure
the machine has enough memory to
spare.
2. Set the default machine folder.
!
Espressif
!/!7 21
2017.05

!
2. Compiling ESP8266_NONOS_SDK
•Create a new folder, for example, D:
\VM.
•Select File > Preferences, and the
system will show the dialog box 👉.
•In the General tab, set the location
for the virtual machine in Default
Machine Folder, for example, D:
\VM.
💬Tip:
ESP8266’s virtual machine takes up
much space (RAM). Please make sure
the machine has enough memory to
spare.
Steps
Results
3. Import the image file.
•Select File > Import Appliance...,
and a dialog box will show up 👉.
•Select the image file, for example, C:
\ESP8266_lubuntu_20141021.ova,
and click on Next.
•Click Import to confirm the settings.
4. Create a shared folder.
•Create a new folder named D:
\VM\share.
•Select Machine > Settings >
Shared Folders…, and a dialog box
will show up 👉.
•Select the shared folder in Machine
Folders, for example, D:\VM\share.
Espressif
!/!8 21
2017.05

!
2. Compiling ESP8266_NONOS_SDK
2.3. Compiling Process
1. Start the virtual machine. Run LXTerminal on the desktop.
2. Copy the ESP8266_NONOS_SDK to the shared folder.
5. Run the virtual machine.
•After importing, a virtual machine
named ESP8266_lubuntu shows up
👉.
•Double-click on ESP8266_lubuntu
or Start to power on the virtual
machine.
•The system shows the ESP8266
virtual machine 👉.
•If the virtual machine enters idle
mode and is locked, a dialog box like
the one below👇 will show up. This
is where the users enter the
password: espressif.
!
•Double-click on LXTerminal to start
compiling applications. For more
details please refer to Chapter 2.3.
Espressif
!/!9 21
2017.05

!
2. Compiling ESP8266_NONOS_SDK
3. Mount the shared directory to the virtual machine.
Steps
Result
•Copy the ESP8266_NONOS_SDK folder to the
shared directory, for example, D:\VM\share.
•Copy the
ESP8266_NONOS_SDK\examples\at folder to
the directory D:
\VM\share\ESP8266_NONOS_SDK, as shown
in the figure on the right 👉.
Steps
Result
•Execute command ./mount.sh in the
LXTerminal.
•Input the password espressif."
Shared folder mounting is completed.
•Open the shared directory
ESP8266_NONOS_SDK in the virtual machine
and check if the mounting has been successful.
- If successful, the directory contains files as
the figure on the right 👉 shows.
- If not, the directory will be empty and users
will need to repeat the previous step.
Espressif
!/!10 21
2017.05

!
2. Compiling ESP8266_NONOS_SDK
4. Change the directory to /Share/ESP8266_NONOS_SDK/at in the LXTerminal.
5. After compilation, the binaries generated and their corresponding download addresses
in the flash memory will be shown as follows:
Supportboot_v1.4and+
Generateuser1.2048.new.5.binsuccessfullyinfolderbin/upgrade.
boot.bin------------>0x00000
user1.2048.new.5.bin--->0x01000
!!!
6. The AT binaries generated can be downloaded to the ESP-LAUNCHER (refer to Section
1.3 ) and run.
Steps
Result
•In the LXTerminal, execute the command: "
cd/home/esp8266/Share/ESP8266_NONOS_SDK/at
•Then execute command: "
./gen_misc.sh!
to start compiling.
•For example, the options for STEP 1 ~ 5 can be:
1, 1, 2, 0, 5.
📖 Note:
For more details on compiling, please refer to ESP8266 SDK Getting Started Guide.
📖 Note:
Users can open the /home/esp8266/Share/ESP8266_NONOS_SDK/bin/upgrade directory and check the
binaries compiled.
Espressif
!/!11 21
2017.05

!
3. Compiling ESP8266_RTOS_SDK
3. Compiling
ESP8266_RTOS_SDK
3.1. Compiling Process
1. Download ESP8266_RTOS_SDK from:
https://github.com/espressif/ESP8266_RTOS_SDK
ESP8266_IOT_PLATFORM is a demo application based on ESP8266_RTOS_SDK.
Download from: https://github.com/espressif/ESP8266_IOT_PLATFORM
2. Copy ESP8266_IOT_PLATFORM and ESP8266_RTOS_SDK to the shared folder.
3. Start the virtual machine. Run LXTerminal.
Steps
Result
Copy ESP8266_RTOS_SDK and
ESP8266_IOT_PLATFORM to the shared folder,
for example, D:\VM\share as shown on the
right👉.
Steps
Result
•Start ESP8266 virtual machine 👉.
-If the virtual machine is locked, please enter
the password: espressif to unlock it.
•Double-click on LXTerminal to start the
compilation.
Espressif
!/!12 21
2017.05

!
3. Compiling ESP8266_RTOS_SDK
4. Mount the shared directory to the virtual machine.
5. Modify the file ESP8266_IOT_PLATFORM/gen_misc.sh. Set the variable PATH to point
to the SDK and binaries.
6. Modify ESP8266_IOT_PLATFORM/makefile.
Steps
Result
•Execute command ./mount.sh in the
LXTerminal.
•Input the password: espressif."
Shared folder mounting is completed.
•Open the shared directory
ESP8266_RTOS_SDK in the virtual machine
and confirm if the mounting has been
successful.
- If successful, the directory contains files as
shown in the figure on the right 👉.
- If not, the directory will be empty, and users
will need to repeat the previous step.
Steps
Result
•SDK_PATH: the path of ESP8266_RTOS_SDK
•BIN_PATH: the path where the generated
binaries are stored after compilation
•Please see the figure on the right 👉.
Steps
Result
Modify the LINKFLAGS_eagle.app.v6area in the
ESP8266_IOT_PLATFORM/makefile by:
-Deleting -lminic
-Adding -lcirom and -lmirom
Espressif
!/!13 21
2017.05

!
3. Compiling ESP8266_RTOS_SDK
7. Switch to /Share/ESP8266_IOT_PLATFORM in the LXTerminal.
8. After compilation, the binaries generated and their download addresses in the flash
memory will be shown as follows:
Supportboot_v1.4and+
Generateuser1.1024.new.2.binsuccessfullyinBIN_PATH
boot.bin------------>0x00000
user1.1024.new.2.bin--->0x01000
!!!
9. Download the generated binaries to the ESP-LAUNCHER and run.
Steps
Result
•Execute the command:"
cd/home/esp8266/Share/ESP8266_IOT_PLATFORM
•Then execute the command:"
./gen_misc.sh!
to start compiling.
📖 Note:
For more details on compilation, please refer to ESP8266 SDK Getting Started Guide.
📖 Note:
Users can open the /home/esp8266/Share/ESP8266_RTOS_SDK/bin directory and check the binaries
compiled.
📖 Note:
The default baud rate of ESP8266 is 74880.
Espressif
!/!14 21
2017.05

!
3. Compiling ESP8266_RTOS_SDK
3.2. ESP8266_RTOS_SDK Architecture
!
Figure 3-1. ESP8266_RTOS_SDK Architecture
Application Framework & Service
Firmware
Upgrade HTTP Client HTTP Server
Cloud
Protocol
Application
(application logic, configurations and policies)
Low MAC
High MAC
Low Level Control and Physical Abstract Layer
Wi-Fi Control Interface
RTOS
ESP
Protocols TCP/IP Power
Management mDNS TLS/SSL XML/
cJSON
Restful Web
Services
Espressif
!/!15 21
2017.05

!
4. Common Debug Methods
4. Common Debug Methods
4.1. Common Debug Methods
4.1.1. Add UART Output Logs
For ESP8266_NONOS_SDK, users can add debug logs as below:
os_printf("SDKversion:%s\n",system_get_sdk_version());
For ESP8266_RTOS_SDK, users can add debug logs as below:
printf("SDKversion:%s\n",system_get_sdk_version());
4.1.2. Debug Fatal Exception
If a fatal exception occurs, the UART output logs will be shown as below:
Fatalexception(28):
epc1=0x4025bfa6,epc2=0x00000000,epc3=0x00000000,excvaddr=0x0000000f,depc=0x00000000
The debugging steps are as follows:
1. Find the .s file that corresponds to the firmware that is currently running.
For example, if eagle.flash.bin and eagle.irom0text.bin are running, then the
corresponding file is eagle .s.
2. Locate the address of epc1 (in the form of 0x40XXXXXX) in the .s file to find the target
function.
3. Add the UART logs before and after the target function to debug the fatal exception
problem.
Espressif
!/!16 21
2017.05

!
5. Downloading Firmware into the ESP-WROOM-02
5. Downloading Firmware into the
ESP-WROOM-02
Please follow the steps below to download firmware into ESP-WROOM-02.
1. ESP-WROOM-02 is the official ESP8266 module provided by Espressif Systems. Lead
out the pins of ESP-WROOM-02, as shown in Table 5-1.
2. Connect ESP-WROOM-02 to the USB-to-TTL converter, using Dupont lines, as shown
in Figure 5-1.
! !
Figure 5-1. ESP-WROOM-02 Download Mode
3. Connect the USB-to-TTL converter to the PC.
4. Download firmware to flash with the ESP8266 Flash Download Tool.
Table 5-1. ESP-WROOM-02 Pins
Pin
Pin status
Figure
EN
Pull up
3V3
3.3V power supply (VDD)
IO15
Pull down
IO0
UART Download mode: pull down;
FLASH Boot mode: floating/pull up
GND
GND
RXD
UART Download Rx
TXD
UART Download Tx, floating/pull up
!
EN
3V3
ESP-WROOM-02
3V3
TXD
RXDTXD
RXD
GNDGND
IO15 IO0
USB-to-TTL converter
PC
Espressif
!/!17 21
2017.05

!
5. Downloading Firmware into the ESP-WROOM-02
5. After downloading, set IO0 as floating or pull up and switch ESP-WROOM-02 to
working mode.
6. Power on ESP-LAUNCHER again and the chip will read and run programs from the
flash.
📖 Note:
On how to download firmware, please refer to Section 1.3.
📖 Note:
IO0 is an internal pull-up pin. For more information on the ESP-WROOM-02 hardware, please refer to
ESP8266 System Description and ESP-WROOM-02 Datasheet.
Espressif
!/!18 21
2017.05

!
Appendix A
A. Appendix—Learning
Resources
A.1. Must-Read Documents
•ESP8266EX Datasheet
Description: This document introduces the specifications of ESP8266EX, including an
overview of its features, protocols, technical parameters and applications. It also
provides ESP8266EX’s pin layout and the relevant description, as well as major
functional modules and protocols applied on ESP8266EX (CPU, flash and memory,
clock, radio, Wi-Fi, and low-power management). Furthermore, it provides a description
of peripheral interfaces integrated on ESP8266EX, lists the electrical data of ESP8266EX
and illustrates the package details for ESP8266EX.
•ESP8266 Hardware Resources
Description: This zip package includes the manufacturing specifications of the ESP8266
board and the modules, manufacturing bill of materials (BOM) and schematics.
•ESP8266 Non-OS SDK IoT_Demo Guide
Description: This document provides simple demo implementations of three types of
smart devices: Smart Lights, Smart Power Plugs, and Sensor Devices. It also
introduces the readers to curl toolkits, functions in LAN and WAN.
•ESP8266 RTOS SDK Programming Guide
Description: This document provides sample codes based on ESP8266_RTOS_SDK,
including basic examples, networking protocol examples and advanced examples.
•ESP8266 AT Command Examples
Description: This document introduces some specific examples of using Espressif’s AT
commands, including setting up single connection using ESP8266 as a TCP client,
setting up UDP transmission and transparent transmission, and setting up multiple
connection using ESP8266 as a TCP server.
•ESP8266 AT Instruction Set
Description: This document provides lists of AT commands based on
ESP8266_NONOS_SDK, including user-defined AT commands, basic AT commands,
Wi-Fi AT commands and TCP/IP-related AT commands. It also introduces the
downloading of AT firmware into flash.
•ESP8266 Non-OS SDK API Reference
Description: This document lists ESP8266_NONOS_SDK APIs, and provides an
overview of the ESP8266_NONOS_SDK. It also introduces the readers to system APIs,
Espressif
!/!19 21
2017.05

!
Appendix A
TCP/UDP APIs, mesh APIs, application-specific APIs, definitions and data structures, as
well as APIs for peripheral interfacing.
•ESP8266 RTOS SDK API Reference
Description: This document lists ESP8266_RTOS_SDK APIs, including functions for Wi-
Fi-related APIs, and boot APIs, etc.
•FAQ
A.2. Must-Have Resources
•ESP8266 SDKs
Description: This webpage provides links to the latest version of the ESP8266 SDK as
well as the older ones.
•RTOS Sample Code
Description: This webpage provides sample code for the commonly-used functions.
•Non-OS Sample Code
Description: This webpage provides sample code for the commonly used functions.
•ESP8266 Tools
Description: This webpage provides links to the ESP8266 flash download tools and
ESP8266 performance evaluation tools.
•ESP8266 APK
•ESP8266 Certification and Test Guide
•ESP8266 BBS
•ESP8266 Resources!
Espressif
!/!20 21
2017.05

Disclaimer and Copyright Notice
Information in this document, including URL references, is subject to change without
notice.
THIS DOCUMENT IS PROVIDED AS IS WITH NO WARRANTIES WHATSOEVER,
INCLUDING ANY WARRANTY OF MERCHANTABILITY, NON-INFRINGEMENT, FITNESS
FOR ANY PARTICULAR PURPOSE, OR ANY WARRANTY OTHERWISE ARISING OUT
OF ANY PROPOSAL, SPECIFICATION OR SAMPLE.
All liability, including liability for infringement of any proprietary rights, relating to use of
information in this document is disclaimed. No licenses express or implied, by estoppel or
otherwise, to any intellectual property rights are granted herein.
The Wi-Fi Alliance Member logo is a trademark of the Wi-Fi Alliance. The Bluetooth logo is
a registered trademark of Bluetooth SIG.
All trade names, trademarks and registered trademarks mentioned in this document are
property of their respective owners, and are hereby acknowledged.
Copyright © 2017 Espressif Inc. All rights reserved.
Espressif IOT Team"
www.espressif.com
Products related to this Datasheet
IC RF TXRX+MCU WIFI 32VFQFN
ESP-WROOM-02D EVAL BOARD
ESP-WROOM-02U EVAL BOARD
EVAL BOARD FOR ESP8266EX
IC RF TXRX+MCU WIFI 32VFQFN
IC RF TXRX+MCU WIFI 32VFQFN