CT4024 Manual Datasheet by Cal Test Electronics

View All Related Products | Download PDF Datasheet
Cal Test ELECTRONICS
CT4024
User Manual
Cal Test ELECTRONICS
800-572-1028 caltestelectronics.com 1
Safety Summary
WARNING CAUTION
To avoid personal injury and/or product damage, review and comply
with the following safety precautions. These precautions apply to both
operating and maintenance personnel and must be followed during all
phases of operation, service, and repair of this instrument.
Only qualified personnel should use this probe. This high voltage
probe is designed to be used by personnel who are trained, experienced,
or otherwise qualified to recognize hazardous situations and who are
trained in the safety precautions necessary to avoid possible injury when
using such a device.
This instrument is intended for usage within Measurement Category I
(CAT I) only.
Do not exceed 60 seconds of contact with high voltage. When
making contact between this probe and any circuit with voltages ≥8 kV
DC, ≥5 kVrms AC, or ≥15 kVpk-pk AC, wait for 5 minutes between such
measurements.
Do not work alone when working with high voltages.
Do not apply to the input any potential that exceeds the maximum
rating of the probe.
For your own safety, inspect the probes for cracks and frayed or broken
leads before each use. If defects are noted, DO NOT USE the probe.
Hands, shoes, floor and work bench must be dry.
Avoid making measurements under humidity, dampness or other
environmental conditions that might affect safety.
Turn the high voltage source off before connecting or disconnecting
the probe whenever possible.
The probe body should be kept clean and free of any conductive
contamination.
Do not remove the probe casing. Removal of the probe’s casing may
800-572-1028 caltestelectronics.com 2
expose you to electric shock.
Keep fingers behind the probe’s finger guard during use.
Always properly ground the probe with the lead before contacting high
voltage circuits with the probe tip. Always disconnect the probe tip from
high voltage circuits before disconnecting the ground lead. Do not connect
the probe ground lead to any point which is at a potential other than earth
ground.
Use only on test instruments where the chassis or return lead is
properly grounded.
Use only in office-type indoor setting
zThe instrument is designed to be used in office-type indoor
environments. Do not operate the instrument:
zIn the presence of noxious, corrosive, or flammable fumes,
gases, vapors, chemicals, or finely-divided particulates.
zIn environments where there is a danger of any liquid being
spilled on the instrument.
zIn air temperatures exceeding the specified operating
temperatures.
zIn atmospheric pressures outside the specified altitude limits or
where the surrounding gas is not air.
Use in an indoor Pollution Degree 2 environment. Measurements made
by this instrument may be outside specifications if the instrument is used
in non-office-type environments. Such environments may include rapid
temperature or humidity changes, sunlight, vibration and/or mechanical
shocks, acoustic noise, electrical noise, strong electric fields, or strong
magnetic fields.
Not for critical applications. This instrument is not authorized for use in
contact with the human body or for use as a component in a life-support
device or system.
Hazardous voltages may be present in unexpected locations in
circuitry being tested when a fault condition in the circuit exists.
Do not substitute parts that are not approved by Cal Test Electronics
or modify this instrument. Return the instrument to Cal Test Electronics
Iii? CE Cal Test ELECTRONICS
800-572-1028 caltestelectronics.com 3
for service and repair to ensure that safety and performance features are
maintained.
A WARNING statement calls attention to an operating procedure,
practice, or condition, which, if not followed correctly, could result in injury
or death to personnel.
A CAUTION statement calls attention to an operating procedure, practice,
or condition, which, if not followed correctly, could result in damage to or
destruction of parts or the entire product.
Compliance Statements
Disposal of Old Electrical & Electronic Equipment
(Applicable in the European Union and other European
countries with separate collection systems). This product is
subject to Directive 2012/19/EU of the European Parliament
and the Council of the European Union on waste electrical
and electronic equipment (WEEE), and in jurisdictions
adopting that Directive, is marked as being put on the market
after August 13, 2005, and should not be disposed of as
unsorted municipal waste. Please utilize your local WEEE
collection facilities in the disposition of this product and
otherwise observe all applicable requirements.
800-572-1028 caltestelectronics.com 4
1 Introduction
Overview
The Elditest CT4024 is an 8 kV High Voltage divider probe for use with
both digital and analog oscilloscopes.
Features
zMeasures up to: 8 kV (DC + ACpk) or 6 kVrms AC
z40 MHz bandwidth
zVoltage dividing of 1000:1
zFrequency compensation
800-572-1028 caltestelectronics.com 5
2 Using the Probe
1. Connect the probe to the BNC input of the oscilloscope.
2. Select the desired volts/division range on your oscilloscope.
3. If possible, always turn the high voltage source off before
connecting or disconnecting the probe.
4. Connect the divider probe ground lead (alligator clip) to a good
earth ground or reliable chassis ground.
5. Before turning on the high voltage source, be certain the
operator is not touching any part of the device under test.
6. Turn on the high voltage source.
7. You will now be able to analyze the voltage waveform on your
oscilloscope.
8. Turn off the high voltage source.
9. Disconnect the High Voltage Probe from the high voltage source
BEFORE disconnecting the ground clip lead.
Chlfint ELECTRONICS UUUUUUUU nnnnnnn :
800-572-1028 caltestelectronics.com 6
3 Frequency Compensation
Proper compensation of the probe is required to assure amplitude
accuracy of the waveform being measured by matching the probe to
the oscilloscope’s input capacitance. Compensation should be adjusted
whenever the probe is connected to, or transferred between, oscilloscopes.
The procedure is the same as for a x10 passive probe.
zConnect the probe to the oscilloscope.
zConnect probe tip to square-wave generator.
zAdjust the square wave generator for 10 V amplitude.
zAdjust the oscilloscope for a time base of 500 µs/div.
zTurn trimmer (Figure 1) to adjust the compensation on the probe
making a flat pulse top.
Figure 1: Trimmer on BNC
Frequency Compensation Trimmer
800-572-1028 caltestelectronics.com 7
Figure 2 shows how over- and under-compensated pulse responses
will look.
Figure 2: Over/Under Compensation
Figure 3 shows a perfectly compensated probe.
Figure 3: Good Compensation
Cal Test ELECTRONICS
800-572-1028 caltestelectronics.com 8
4 Specifications
All specifications apply to the unit after a temperature stabilization time
of 15 minutes over an ambient temperature range of 25 °C ± 5 °C.
CT4024
8 kV High Voltage Probe
Operating Parameters
Maximum Input Voltage
(CAT I)
8 kV (DC + ACpk)
6 kVrms AC
Division Ratio 1000:1
Bandwidth 40 MHz (-3 dB)
Compensation Range 5 pF to 50 pF
Temperature Coefficient ≤200 ppm/ºC
Input Resistance 100 MΩ ± 5%
Rise Time ≤9 ns
Accuracy
DC Volts ±3% (below 8 kV)
AC Volts ±3% at 1 kHz
±3 dB 0 to 40 MHz
General
Cable Length 6.6 ft (2 m)
Designed for Use in Pollution Degree 2
Operating Environment 32ºF to 122ºF (0ºC to 50ºC)
Storage Temperature -4ºF to 158ºF (-20ºC to 70ºC)
Humidity ≤80% relative humidity at 104ºF (40ºC)
Dimensions 8.3 in (21 cm)
Weight 0.40 lbs (180 g)
Warranty One-year warranty
Specifications are subject to change without notice. To ensure the most
current version of this manual, please download the current version
from our website: caltestelectronics.com.
Cal Test ELECTRONICS 24 Ma num Wor ng Voltage Dera ng Curve «onKv ZDKV k7 VOKV < +="" e="" \="" tu]="" \‘="" 3?="" va="" t:=""> ~\\\\\\ \\ 100v ‘ \\\“‘ wKHz 10KH1 VOOKHI 1MHz IOMHz 100MHz Frequency
800-572-1028 caltestelectronics.com 9
5 Voltage Derating Curve
WARNING
When measuring higher frequency signals, be sure to comply with the
Voltage vs Frequency Derating Curve.
Figure 4: Voltage Derating Curve
Cal Test ELECTRONICS
800-572-1028 caltestelectronics.com 10
6 Cleaning
Clean only the exterior probe body and cables. Use a soft cotton cloth
lightly moistened with a mild solution of detergent and water. Do not
allow any portion of the probe to be submerged at any time.
WARNING
Dry the probe thoroughly before attempting to make voltage
measurements.
CAUTION Do not subject the probe to solvents or solvent fumes as
these can cause deterioration of the probe body and cables.
7 Service & Warranty Information
Limited One-Year Warranty
Cal Test Electronics warrants this product to be free from defective
material or workmanship for a period of 1 year from the date of original
purchase. Under this warranty, Cal Test Electronics is limited to
repairing the defective device when returned to the factory, shipping
charges prepaid, within the warranty period.
Units returned to Cal Test Electronics that have been subject to abuse,
misuse, damage, or accident, or have been connected, installed, or
adjusted contrary to the instructions furnished by Cal Test Electronics,
or that have been repaired by unauthorized persons, will not be
covered by this warranty.
Cal Test Electronics reserves the right to discontinue models, change
specifications, price, or design of this device at any time without notice
and without incurring any obligation whatsoever.
The purchaser agrees to assume all liabilities for any damages and/or
bodily injury which may result from the use or misuse of this device by
the purchaser, his employees, or agents.
800-572-1028 caltestelectronics.com 11
This warranty is in lieu of all other representations or warranties
expressed or implied and no agent or representative of Cal Test
Electronics is authorized to assume any other obligation in connection
with the sale and purchase of this device.
Service
If you have a need for calibration or repair services, technical, or sales
support, please contact us:
22820 Savi Ranch Parkway
Yorba Linda, CA 92887
800-572-1028 or 714-221-9330
caltestelectronics.com
800-572-1028 caltestelectronics.com 12
Notes
800-572-1028 caltestelectronics.com 13
800-572-1028 caltestelectronics.com 14
800-572-1028 caltestelectronics.com 15

Products related to this Datasheet

OSCOPE PROBE X1K 40MHZ 100M