Configurable Logic Cell Tip N Tricks Datasheet by Microchip Technology
View All Related Products | Download PDF Datasheet
2012 Microchip Technology Inc. DS41631B-page 1
Configurable Logic Cell Tips ’n Tricks
TIPS ‘N TRICKS INTRODUCTION
Microchip continues to provide innovative products that
are smaller, faster, easier to use and more reliable.
Flash-based PIC® microcontrollers (MCUs) are used in
a wide range of everyday products from smoke
detectors to industrial, automotive and medical
products.
The PIC16(L)F150X and PIC10(L)F32X families of
devices with on-chip configurable logic cells merge all
the advantages of the PIC® MCU architecture and the
flexibility of Flash program memory with the functional-
ity of a configurable digital logic cell. Together, they
form a low-cost building block with resource savings
and external component reduction.
The flexibility of Flash and an excellent development
tool suite, including a low-cost In-Circuit Debugger, In-
Circuit Serial ProgrammingTM (ICSPTM) and CLC
Configuration Tool GUI, make these devices ideal for
just about any embedded control application.
The following series of Tips ‘n Tricks can be applied to
a variety of applications to help make the most of digital
logic functions using a PIC MCU with on-chip
configurable logic.
CLC OVERVIEW
Input Selection
For all CLC modules, there are eight signals available
as inputs to the configurable logic cell, and these eight
input signals may vary from device to device. Neverthe-
less, only four can be selected at any one time. This is
done via four 8-input multiplexers, used to pass the
input signals on to the data gating stage of the CLC.
Input signals are selected with the CLCxSEL0 and
CLCxSEL1 registers, as shown in Figure 1.
FIGURE 1: CLC CONFIGURATION
Configurable Logic Cell (CLC)

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 2 2012 Microchip Technology Inc.
Data Gating
The outputs from the input multiplexers are directed to
the data gating stage of the CLC. The data gates can
be configured to direct each input signal as inverted or
non-inverted data signals. These signals are then
ANDed together in each gate. Finally, each gates
output can be inverted before going on to the logic
function stage of the CLC.
The basic logic that can be obtained in each gate is
summarized in Ta b l e 1 and Figure 2.
FIGURE 2: CLC DATA GATING LOGIC
LOGIC FUNCTION SELECTION
The outputs from the four data gates are now inputs
into the logic function selection stage of the CLC. Here,
the data gate outputs can be gated down to one output
signal from a selection of eight logic functions. These
eight logic functions are shown in Figure 3 through
Figure 10.
TABLE 1: DATA GATING LOGIC
CLCxGLS(0-3) Registers LCxGyPOL bits Gate Logic
Inverted 55h 1AND
55h 0NAND
Non-Inverted AAh 1NOR
AAh 0OR
Not Connected 00h 0Logic 0
00h 1Logic 1
AND
NAND
NOR
OR

2012 Microchip Technology Inc. DS41631B-page 3
Configurable Logic Cell Tips ’n Tricks
FIGURE 3: AND-OR
FIGURE 4: OR-XOR

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 4 2012 Microchip Technology Inc.
FIGURE 5: 4 – INPUT AND
FIGURE 6: SR LATCH

2012 Microchip Technology Inc. DS41631B-page 5
Configurable Logic Cell Tips ’n Tricks
FIGURE 7: 1 – INPUT D FLIP-FLOP WITH SET AND RESET
FIGURE 8: 2 – INPUT D FLIP-FLOP WITH RESET

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 6 2012 Microchip Technology Inc.
FIGURE 9: J – K FLIP-FLOP WITH RESET
FIGURE 10: 1 – INPUT TRANSPARENT LATCH WITH SET AND RESET

2012 Microchip Technology Inc. DS41631B-page 7
Configurable Logic Cell Tips ’n Tricks
OUTPUT CONTROL
The last stage of the CLC is the output control stage.
Here the output signal from the logic function selection
stage can be inverted, or not, and sent to the device
output pin or sent internally to other peripherals. Also,
an interrupt can be generated upon a change in the
CLC output signal. This interrupt can be set to occur on
the rising or falling edge of the CLC output signal.
FIGURE 11: 1 – INPUT TRANSPARENT LATCH WITH SET AND RESET

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 8 2012 Microchip Technology Inc.
TIP 1: REROUTING AN OUTPUT PIN
How often have you needed to move a signal on one
pin of a PIC MCU to another? Often, this will have to be
done by extra source code that eats up device
resources or by physically adding a jumper wire that
does not look very good. This tip presents a simple
method of rerouting one device pin to another pin on
the same device internally, using the CLC module
without using up precious resources.
Although there are some limits placed on which pins
can be routed to which locations, the input pin must be
one of the CLC inputs and the destination pin must be
one of the CLC output pins.
TABLE 2: EXAMPLE ALLOCATION TABLE
This device has two CLC modules, see Table 2. CLC1
and CLC2. CLC1 has inputs on pins RA3 and RC7,
either one of these pins can be moved to RA2 or RC5
(RC5 requires the use of the APFCON register). Like-
wise, when using CLC2, it has inputs on pins RC3 and
RC4, either one of these pins can be moved to RC0
only.
I/O
20-Pin PDIP/SOIC/SSOP
20-Pin QFN
A/D
Reference
CWG
NCO
CLC
Timers
PWM
Interrupt
Pull-up
Basic
RA0 19 16 AN0 — — — — — — IOC YICSPDAT
RA1 18 15 AN1 VREF+ — — — — — IOC YICSPCLK
RA2 17 14 AN2 —CWG1FLT —CLC1(1) T0CKI PWM3 INT/
IOC
Y —
RA3 4 1 — — — — CLC1IN0 — — IOC YMCLR
VPP
RA4 320 AN3 — — — — T1G —IOC YCLKOUT
RA5 219 — — — NCO1CLK —T1CKI —IOC YCLKIN
RB4 13 10 AN10 — — — — — — IOC Y —
RB5 12 9AN11 — — — — — — IOC Y —
RB6 11 8 — — — — — — — IOC Y —
RB7 10 7 — — — — — — — IOC Y —
RC0 16 13 AN4 — — — CLC2 — — — — —
RC1 15 12 AN5 — — NCO1(1) — — PWM4 — — —
RC2 14 11 AN6 — — — — — — — — —
RC3 7 4 AN7 — — — CLC2IN0 —PWM2 — — —
RC4 6 3 — — CWG1B —CLC2IN1 — — — — —
RC5 5 2 — — CWG1A —CLC1(2) —PWM1 — — —
RC6 8 5 AN8 — — NCO1(2) — — — — — —
RC7 9 6 AN9 — — — CLC1IN1 — — — — —
VDD 118 — — — — — — — — — VDD
VSS 20 17 — — — — — — — — — VSS
Note 1: Default location for peripheral pin function. Alternate location can be selected using the APFCON register.
2: Alternate location for peripheral pin function selected by the APFCON register.

2012 Microchip Technology Inc. DS41631B-page 9
Configurable Logic Cell Tips ’n Tricks
TIP 2: MANCHESTER ENCODER
Manchester encoding is a versatile line encoding
method, which is widely used. When the EUSART is
used to transmit data, various mechanisms such as
interrupts and buffers are available to free up resources
on the CPU. To date, however, it was required to either
perform a bit-bang transmission or use external
hardware to take this output signal and encode it in
Manchester format.
FIGURE 12: MANCHESTER-ENCODED SIGNAL
This tip presents a method to produce a Manchester-
encoded output signal by using the SPI port in
Synchronous mode with the CLC. By combining the
SPI clock with the SPI data using the CLC, a Manches-
ter-encoded signal can be created in hardware with no
overhead and no external components required to do
the modulation.
Configure the CLC as shown in Figure 13. The output
will be a Manchester-encoded version of the data sent
via SPI in Master mode.
FIGURE 13: CLC CONFIGURED FOR MANCHESTER ENCODING
Clock
Bit Stream
Manchester-
Encoded Output
Bit Stream
Clock Manchester-Encoded Output
10 1 0 0 1 1

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 10 2012 Microchip Technology Inc.
TIP 3: FREQUENCY DIVIDER
Frequency dividers are commonly used building blocks
for more complex applications.
By negating the CLC4OUT signal when feeding it into
D, we are effectively tapping out Q. The flip-flop clocks
this input through to the output on the positive edge of
the next external clock, causing the output to toggle
once for every positive edge coming in from the
external signal. This results in the input clock being
divided by two at the output. Using the CLC as a D flip-
flop, the user can create a simple frequency divider by
connecting it up as follows. See Figure 14.
FIGURE 14: CLC CONFIGURED FOR FREQUENCY DIVIDER

2012 Microchip Technology Inc. DS41631B-page 11
Configurable Logic Cell Tips ’n Tricks
TIP 4: CONDITIONAL WAKE FROM
SLEEP
In applications where power use is critical, it is common
to put the microcontroller to Sleep in order to save
power, and wake it up only when a specific event has
occurred which requires attention.
If the condition we are looking for requires a number of
signals to represent a specific state, it often results in
the CPU waking from Sleep due to a pin change, only
to check the condition and realize that the other inputs,
which constitute the specific condition, have not
occurred, resulting in a waste of power.
This tip describes how to wake the microcontroller from
Sleep when a combination of things are true.
Since the CLC keeps running even when the device
has been placed in Sleep mode, and the device can be
woken from Sleep by an interrupt created by a CLC
output changing, it is possible to conditionally wake the
device from Sleep. The CLC can be configured to
perform a number of logical operations such as OR,
XOR or AND operations on input signals, and even
combine this with stateful behavior by incorporating
flip-flops, waking the device from Sleep only when a
very specific combination occurs.

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 12 2012 Microchip Technology Inc.
TIP 5: FAST PULSE DETECTOR/
PULSE EXTENDER
When using a microprocessor to do pulse counting or
simply react to a condition where an input pin is
presented with a very short one-shot pulse, it is often a
problem that these small pulses are missed, resulting
in incorrect behavior.
While it is possible to solve this problem by using an
interrupt-on-change mechanism, many applications
have to operate in deterministic time (real time) and are
thus prevented from using interrupts. In this case,
inputs need to be polled at a specific time to determine
the value, making it impractical to count short pulses.
This tip describes a way to detect a clock edge on an
external pin and hold it, even if the input changes back
to the original state very quickly. By Configuring the
CLC to clock the pulse edge into a D flip-flop, as shown
in Figure 15, it is possible to save the pulse for an indef-
inite amount of time, allowing the microprocessor to
read and react to the impulse at its own leisure.
FIGURE 15: CLC CONFIGURED TO CLOCK A D FLIP-FLOP
This will solve the problem in all cases where multiple
pulses are not expected in quick succession. This
same technique also allows for the debouncing of a
contact that needs to be read, ensuring that multiple
events are not triggered by a single contact change.
Variation:
By adding an input to the reset line of the D flip-flop and
feeding this back from the output via a RC filter, it is
possible to simply extend the pulse instead of continu-
ing the signal indefinitely.

2012 Microchip Technology Inc. DS41631B-page 13
Configurable Logic Cell Tips ’n Tricks
TIP 6: SIGNAL THRESHOLD AND
HOLD CIRCUIT
Interfacing a digital device, such as a CPU, with an
analog device, such as a photodiode, can be challeng-
ing. As the output signal will be offset by the ambient
light, which may vary widely between different
conditions such as being indoors, or outdoors in direct
sunlight. These conditions can cause the entire upper
(logic 1), or the entire lower (logic 0) part of the signal
to fall within the undefined range on the device
(between VIN0max and VIN1min). On many devices,
these values can be significantly far apart, as digital
electronics are designed to operate at discreet values
of ‘1’ and ‘0’, and not in between.
In order to overcome this problem, it is necessary to
change the threshold where the decision is made
whether the signal represents a ‘0’ or a ‘1’, and elimi-
nate as much as possible of the undefined region in
between the two. This can be accomplished by using
an on-chip comparator to sample the signal, by feeding
the non-inverting input signal to the comparator from an
internal Digital-to-Analog Converter (DAC) peripheral.
This tip presents a simple method of sampling the input
signal with a precise threshold, overcoming the
problem of a signal floating in the undefined region of a
normal input pin. The comparator is set up to sample
and hold the input signal precisely at the bias point
using the internal DAC. The CLC is configured as a D
flip-flop to sample and hold the value as follows.
FIGURE 16: CLC CONFIGURED AS A D FLIP-FLOP TO SAMPLE AND HOLD VALUES
For example, when decoding a quadrature-encoded
input signal from a optical rotary encoder, a timer can
be set up to sample both inputs in this fashion and
adjust for the ambient offset by adjusting the bias
voltage from the DAC.

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 14 2012 Microchip Technology Inc.
TIP 7: QUADRATURE DECODER
Many input devices, such as rotary encoders, provide a
quadrature-encoded output signal, which needs to be
decoded to determine if the device has been turned
and in which direction it has been turned. See
Figure 18.
A common problem with circuits that decode this
quadrature-encoded signal (see Figure 17) occurs
when the input is left between a ‘0’ and a ‘1’, and one
of the two lines is toggled repeatedly, causing the
device to mistakenly detect the dial is still being turned,
while it is in fact, stationary.
FIGURE 17: QUADRATURE-ENCODED
SIGNAL
FIGURE 18: TYPICAL QUADRATURE DECODER CIRCUIT
This tip describes how to use the CLC to decode a
quadrature-encoded input signal such as a rotary
encoder. As seen above, the line connected to the flip-
flop clock toggles repeatedly due to noise if it is left
between a ‘1’ and a ‘0’ level, and will cause the counter
to keep on counting (or “run”) without the turning of the
wheel.
The circuit below (Figures 19, 20, and 21) uses two
D-type flip-flops with a clear input to generate two
separate pulse trains for clockwise and anti-clockwise
rotation. By clearing the output from the line, which is
not used as the clock, we ensure that the circuit will
never “run” in one direction, if the dial is not being
turned.
FIGURE 19: SCHEMATIC OF ROTARY ENCODERS CONNECTION TO THE CLC INPUTS
Using the CLC, the D-type flip-flops needed are
available on-chip with no external components
required. (Note that the CLR input is active-low, so in
the CLC this input needs to be configured as inverted
between D and CLR.)
360°
A
B
12 3 4
LCD
POT
CWGxA
CWGxB Driver
Circuit MAB
VDD VDD
CLC1IN0 RA3
+5 V
DC
2.7k
2.7k 74HC14
56pF
Encoder
Ch. A
+5 V
DC
2.7k
2.7k 74HC14
56pF
Encoder
Ch. B
CLC2IN0 RC3
CLC1IN1 RC7
CLC2IN1 RC4

2012 Microchip Technology Inc. DS41631B-page 15
Configurable Logic Cell Tips ’n Tricks
FIGURE 20: CLC1 CONFIGURATION FOR ROTARY ENCODER SIGNALS
FIGURE 21: CLC2 CONFIGURATION FOR ROTARY ENCODER SIGNALS

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 16 2012 Microchip Technology Inc.
TIP 8: PWM STEERING
Pulse-Width Modulation (PWM) applications can be
challenging, especially if an application needs one
PWM signal in up to four different locations, or up to
four different PWM signals in up to four different
locations.
This tip describes how to use the CLC to steer one or
up to four different PWM signals to up to four different
pins on a device.
The first example will show how to set up all four CLC’s
to output four different PWM signals. The second
example will show how to set up all four CLC’s to output
one PWM signal.
EXAMPLE 1
First, you need a device that has four CLC peripherals,
like the PIC16F1508. Second, set up the CLC2 with the
output of PWM1 as an input, CLC3 with PWM2 as the
input, CLC4 with PWM4 as the input, and CLC1 with
PWM3 as the input. Then, AND-OR the PWM signal to
the specific output pin for each CLC, as shown in
Figures 22, 23, 24 and 25.
FIGURE 22: CLC1 CONFIGURATION FOR EXAMPLE 1

2012 Microchip Technology Inc. DS41631B-page 17
Configurable Logic Cell Tips ’n Tricks
FIGURE 23: CLC2 CONFIGURATION FOR EXAMPLE 1
FIGURE 24: CLC3 CONFIGURATION FOR EXAMPLE 1

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 18 2012 Microchip Technology Inc.
FIGURE 25: CLC4 CONFIGURATION FOR EXAMPLE 1
With the microcontroller configured this way, each
PWM can be set up to output four different PWM
signals. However, what if only one PWM signal is
needed on up to four different output pins? See
Example 2 below.
EXAMPLE 2
Again, using the PIC16F1508 device, only CLC2 will be
set up with the output of PWM1 as the input, and all
other CLC’s will be linked off of CLC2. This will put the
output of PWM1 on four different output pins. See
Figures 26, 27, 28 and 29.

2012 Microchip Technology Inc. DS41631B-page 19
Configurable Logic Cell Tips ’n Tricks
FIGURE 26: CLC2 CONFIGURATION FOR EXAMPLE 2
FIGURE 27: CLC1 CONFIGURATION FOR EXAMPLE 2

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 20 2012 Microchip Technology Inc.
FIGURE 28: CLC3 CONFIGURATION FOR EXAMPLE 2
FIGURE 29: CLC4 CONFIGURATION FOR EXAMPLE 2

2012 Microchip Technology Inc. DS41631B-page 21
Configurable Logic Cell Tips ’n Tricks
TIP 9: GLITCH-FREE CLOCK SIGNAL
A ‘glitch’ is a signal which does not remain active for a
full clock period. If a signal with a glitch feeds the clock
line of numerous latches, some of the latches may get
updated, while others may not. This is clearly a
situation that designers want to avoid.
FIGURE 30: LOGICAL ‘AND’ OF ASYNCHRONOUS PULSE AND SYSTEM CLOCK
For this example, a PIC16F1509 was used because
three of the four available internal CLC modules will be
needed. The NCO will be used as a high speed counter
to increment as long as an external pulse signal is high.
This creates a high-resolution, long-duration counter,
as the NCO counter is a 20-bit wide register. It will take
approximately 16 instruction cycles (4 µs with 16 MHz
clock) for the data to be read and the counter to reset,
so it is necessary to have at least 4 µs of low time
between pulses. A falling edge interrupt flag on CLC2
provides a signal that the pulse width measurement
has been completed. CLC1 setup as an XOR gate will
have the function of taking feedback from the D flip-flop
(CLC2) and inverting the clock, so that it will trigger on
the falling edge once the flip-flop has been set. CLC3
will use the ‘AND’ function to clock the NCO when the
pulse is high. It will do this by creating a new signal that
would only rise on the rising edge of the clock, and only
fall on the falling edge of the clock. This new signal
(CLC2OUT) is then AND’ed with the oscillator clock,
thus insuring a glitch-free output signal. A simplified
schematic for this is shown below (Figure 31).
FIGURE 31: CLC SETUP FOR GLITCH-FREE SIGNAL
Asynchronous input signal
PIC® internal oscillator
Clock signal with glitch
Note: For more detailed information, refer to
application note AN1451 “Glitch-Free
Design Using the Configurable Logic Cell
(CLC)”.
DQ
R
PULSE (RC3)
CLOCK
CLC1OUT
CLC2OUT
GLITCH-FREE
OUTPUT
(CLC3OUT)
CLC1 CLC2 CLC3

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 22 2012 Microchip Technology Inc.
TIP 10: DELAY BLOCK/DEBOUNCER
In this example, the Configurable Logic Cell (CLC) is
being used to implement a delay block/debouncer. The
delay can be set between 2µs and 193 µs, which is
used effectively as a noise discriminator, or for switch
debouncing.
When used as a delay block, the application can be
used to fix low-level timing issues on signals. When
used as a debouncer, it can debounce signals from a
mechanical switch, so that a clean signal can feed
other circuitry.
The Configurable Logic Cell peripheral is used to
produce fast switching on the output (if desired). If the
same application were written using port logic only,
there would be multiple instruction cycles before the
output would change in response to an input. Thus, in
using the CLC, the signal can be routed directly and
only have propagation and gate delay between the
input and output signals.
With the CLC block configured as a pass-through, it is
possible to quickly route signals to the output when no
delay is desired, and the PIC® device core (port
function) will create edge delays when desired. The
MUX (CLC1CON, LC1OE) selects whether the pin is
driven by the CLC or by the port logic (Figure 32).
FIGURE 32: BLOCK DIAGRAM
Note: For detailed information, refer to applica-
tion note AN1450 “Delay Block/
Debouncer”.
0
1
Port Pin
Input
Port Pin
Output
PIC® Device Core PORTA<2>
CLC Block
configured as
pass-through
CLC1CON, LC1OE

2012 Microchip Technology Inc. DS41631B-page 23
Configurable Logic Cell Tips ’n Tricks
RESOURCES
[1] Configurable Logic Cell (CLC) Configuration
Tool User’s Guide, DS41597 at
www.microchip.com.
[2] Configurable Logic Cell (CLC) Configuration
Tool GUI software at www.microchip.com.
[3] Device data sheet for the specific device being
used, at www.microchip.com.

Configurable Logic Cell Tips ’n Tricks
DS41631B-page 24 2012 Microchip Technology Inc.
NOTES:

2012 Microchip Technology Inc. DS41631B-page 25
Information contained in this publication regarding device
applications and the like is provided only for your convenience
and may be superseded by updates. It is your responsibility to
ensure that your application meets with your specifications.
MICROCHIP MAKES NO REPRESENTATIONS OR
WARRANTIES OF ANY KIND WHETHER EXPRESS OR
IMPLIED, WRITTEN OR ORAL, STATUTORY OR
OTHERWISE, RELATED TO THE INFORMATION,
INCLUDING BUT NOT LIMITED TO ITS CONDITION,
QUALITY, PERFORMANCE, MERCHANTABILITY OR
FITNESS FOR PURPOSE. Microchip disclaims all liability
arising from this information and its use. Use of Microchip
devices in life support and/or safety applications is entirely at
the buyer’s risk, and the buyer agrees to defend, indemnify and
hold harmless Microchip from any and all damages, claims,
suits, or expenses resulting from such use. No licenses are
conveyed, implicitly or otherwise, under any Microchip
intellectual property rights.
Trademarks
The Microchip name and logo, the Microchip logo, dsPIC,
FlashFlex, KEELOQ, KEELOQ logo, MPLAB, PIC, PICmicro,
PICSTART, PIC32 logo, rfPIC, SST, SST Logo, SuperFlash
and UNI/O are registered trademarks of Microchip Technology
Incorporated in the U.S.A. and other countries.
FilterLab, Hampshire, HI-TECH C, Linear Active Thermistor,
MTP, SEEVAL and The Embedded Control Solutions
Company are registered trademarks of Microchip Technology
Incorporated in the U.S.A.
Silicon Storage Technology is a registered trademark of
Microchip Technology Inc. in other countries.
Analog-for-the-Digital Age, Application Maestro, BodyCom,
chipKIT, chipKIT logo, CodeGuard, dsPICDEM,
dsPICDEM.net, dsPICworks, dsSPEAK, ECAN,
ECONOMONITOR, FanSense, HI-TIDE, In-Circuit Serial
Programming, ICSP, Mindi, MiWi, MPASM, MPF, MPLAB
Certified logo, MPLIB, MPLINK, mTouch, Omniscient Code
Generation, PICC, PICC-18, PICDEM, PICDEM.net, PICkit,
PICtail, REAL ICE, rfLAB, Select Mode, SQI, Serial Quad I/O,
Total Endurance, TSHARC, UniWinDriver, WiperLock, ZENA
and Z-Scale are trademarks of Microchip Technology
Incorporated in the U.S.A. and other countries.
SQTP is a service mark of Microchip Technology Incorporated
in the U.S.A.
GestIC and ULPP are registered trademarks of Microchip
Technology Germany II GmbH & Co. & KG, a subsidiary of
Microchip Technology Inc., in other countries.
All other trademarks mentioned herein are property of their
respective companies.
© 2012, Microchip Technology Incorporated, Printed in the
U.S.A., All Rights Reserved.
Printed on recycled paper.
ISBN: 9781620766033
Note the following details of the code protection feature on Microchip devices:
• Microchip products meet the specification contained in their particular Microchip Data Sheet.
• Microchip believes that its family of products is one of the most secure families of its kind on the market today, when used in the
intended manner and under normal conditions.
• There are dishonest and possibly illegal methods used to breach the code protection feature. All of these methods, to our
knowledge, require using the Microchip products in a manner outside the operating specifications contained in Microchip’s Data
Sheets. Most likely, the person doing so is engaged in theft of intellectual property.
• Microchip is willing to work with the customer who is concerned about the integrity of their code.
• Neither Microchip nor any other semiconductor manufacturer can guarantee the security of their code. Code protection does not
mean that we are guaranteeing the product as “unbreakable.”
Code protection is constantly evolving. We at Microchip are committed to continuously improving the code protection features of our
products. Attempts to break Microchip’s code protection feature may be a violation of the Digital Millennium Copyright Act. If such acts
allow unauthorized access to your software or other copyrighted work, you may have a right to sue for relief under that Act.
Microchip received ISO/TS-16949:2009 certification for its worldwide
headquarters, design and wafer fabrication facilities in Chandler and
Tempe, Arizona; Gresham, Oregon and design centers in California
and India. The Company’s quality system processes and procedures
are for its PIC® MCUs and dsPIC® DSCs, KEELOQ® code hopping
devices, Serial EEPROMs, microperipherals, nonvolatile memory and
analog products. In addition, Microchip’s quality system for the design
and manufacture of development systems is ISO 9001:2000 certified.
QUALITY MANAGEMENT S
YSTEM
CERTIFIED BY DNV
== ISO/TS 16949 ==

DS41631B-page 26 2012 Microchip Technology Inc.
AMERICAS
Corporate Office
2355 West Chandler Blvd.
Chandler, AZ 85224-6199
Tel: 480-792-7200
Fax: 480-792-7277
Technical Support:
http://www.microchip.com/
support
Web Address:
www.microchip.com
Atlanta
Duluth, GA
Tel: 678-957-9614
Fax: 678-957-1455
Boston
Westborough, MA
Tel: 774-760-0087
Fax: 774-760-0088
Chicago
Itasca, IL
Tel: 630-285-0071
Fax: 630-285-0075
Cleveland
Independence, OH
Tel: 216-447-0464
Fax: 216-447-0643
Dallas
Addison, TX
Tel: 972-818-7423
Fax: 972-818-2924
Detroit
Farmington Hills, MI
Tel: 248-538-2250
Fax: 248-538-2260
Indianapolis
Noblesville, IN
Tel: 317-773-8323
Fax: 317-773-5453
Los Angeles
Mission Viejo, CA
Tel: 949-462-9523
Fax: 949-462-9608
Santa Clara
Santa Clara, CA
Tel: 408-961-6444
Fax: 408-961-6445
Toronto
Mississauga, Ontario,
Canada
Tel: 905-673-0699
Fax: 905-673-6509
ASIA/PACIFIC
Asia Pacific Office
Suites 3707-14, 37th Floor
Tower 6, The Gateway
Harbour City, Kowloon
Hong Kong
Tel: 852-2401-1200
Fax: 852-2401-3431
Australia - Sydney
Tel: 61-2-9868-6733
Fax: 61-2-9868-6755
China - Beijing
Tel: 86-10-8569-7000
Fax: 86-10-8528-2104
China - Chengdu
Tel: 86-28-8665-5511
Fax: 86-28-8665-7889
China - Chongqing
Tel: 86-23-8980-9588
Fax: 86-23-8980-9500
China - Hangzhou
Tel: 86-571-2819-3187
Fax: 86-571-2819-3189
China - Hong Kong SAR
Tel: 852-2401-1200
Fax: 852-2401-3431
China - Nanjing
Tel: 86-25-8473-2460
Fax: 86-25-8473-2470
China - Qingdao
Tel: 86-532-8502-7355
Fax: 86-532-8502-7205
China - Shanghai
Tel: 86-21-5407-5533
Fax: 86-21-5407-5066
China - Shenyang
Tel: 86-24-2334-2829
Fax: 86-24-2334-2393
China - Shenzhen
Tel: 86-755-8203-2660
Fax: 86-755-8203-1760
China - Wuhan
Tel: 86-27-5980-5300
Fax: 86-27-5980-5118
China - Xian
Tel: 86-29-8833-7252
Fax: 86-29-8833-7256
China - Xiamen
Tel: 86-592-2388138
Fax: 86-592-2388130
China - Zhuhai
Tel: 86-756-3210040
Fax: 86-756-3210049
ASIA/PACIFIC
India - Bangalore
Tel: 91-80-3090-4444
Fax: 91-80-3090-4123
India - New Delhi
Tel: 91-11-4160-8631
Fax: 91-11-4160-8632
India - Pune
Tel: 91-20-2566-1512
Fax: 91-20-2566-1513
Japan - Osaka
Tel: 81-66-152-7160
Fax: 81-66-152-9310
Japan - Yokohama
Tel: 81-45-471- 6166
Fax: 81-45-471-6122
Korea - Daegu
Tel: 82-53-744-4301
Fax: 82-53-744-4302
Korea - Seoul
Tel: 82-2-554-7200
Fax: 82-2-558-5932 or
82-2-558-5934
Malaysia - Kuala Lumpur
Tel: 60-3-6201-9857
Fax: 60-3-6201-9859
Malaysia - Penang
Tel: 60-4-227-8870
Fax: 60-4-227-4068
Philippines - Manila
Tel: 63-2-634-9065
Fax: 63-2-634-9069
Singapore
Tel: 65-6334-8870
Fax: 65-6334-8850
Taiwan - Hsin Chu
Tel: 886-3-5778-366
Fax: 886-3-5770-955
Taiwan - Kaohsiung
Tel: 886-7-536-4818
Fax: 886-7-330-9305
Taiwan - Taipei
Tel: 886-2-2500-6610
Fax: 886-2-2508-0102
Thailand - Bangkok
Tel: 66-2-694-1351
Fax: 66-2-694-1350
EUROPE
Austria - Wels
Tel: 43-7242-2244-39
Fax: 43-7242-2244-393
Denmark - Copenhagen
Tel: 45-4450-2828
Fax: 45-4485-2829
France - Paris
Tel: 33-1-69-53-63-20
Fax: 33-1-69-30-90-79
Germany - Munich
Tel: 49-89-627-144-0
Fax: 49-89-627-144-44
Italy - Milan
Tel: 39-0331-742611
Fax: 39-0331-466781
Netherlands - Drunen
Tel: 31-416-690399
Fax: 31-416-690340
Spain - Madrid
Tel: 34-91-708-08-90
Fax: 34-91-708-08-91
UK - Wokingham
Tel: 44-118-921-5869
Fax: 44-118-921-5820
Worldwide Sales and Service
11/29/11
Products related to this Datasheet
IC MCU 8BIT 1.75KB FLASH 8MSOP
IC MCU 8BIT 3.5KB FLASH 14SOIC
IC MCU 8BIT 896B FLASH SOT236
IC MCU 8BIT 14KB FLASH 20QFN
IC MCU 8BIT 448B FLASH SOT236
IC MCU 8BIT 3.5KB FLASH 14SOIC
IC MCU 8BIT 896B FLASH SOT236
IC MCU 8BIT 3.5KB FLASH 14SOIC
IC MCU 8BIT 3.5KB FLASH 14SOIC
IC MCU 8BIT 14KB FLASH 20QFN
IC MCU 8BIT 14KB FLASH 20QFN
IC MCU 8BIT 3.5KB FLASH 16UQFN
IC MCU 8BIT 1.75KB FLASH 8UDFN
IC MCU 8BIT 7KB FLASH 20QFN
IC MCU 8BIT 1.75KB FLASH 8SOIC
IC MCU 8BIT 3.5KB FLASH 16QFN
IC MCU 8BIT 896B FLASH SOT236
IC MCU 8BIT 3.5KB FLASH 14TSSOP
IC MCU 8BIT 3.5KB FLASH 16QFN
IC MCU 8BIT 1.75KB FLASH 8MSOP
IC MCU 8BIT 1.75KB FLASH 8MSOP
IC MCU 8BIT 1.75KB FLASH 8DIP
IC MCU 8BIT 3.5KB FLASH 14SOIC
IC MCU 8BIT 448B FLASH SOT236
IC MCU 8BIT 3.5KB FLASH 14TSSOP
IC MCU 8BIT 14KB FLASH 20SSOP
IC MCU 8BIT 3.5KB FLASH 20SOIC
IC MCU 8BIT 14KB FLASH 20SSOP
IC MCU 8BIT 7KB FLASH 20SSOP
IC MCU 8BIT 7KB FLASH 20SOIC