Microsemi SmartFusion2 Maker Board Available Worldwide Exclusively from Digi-Key

THIEF RIVER FALLS, Minnesota, USA - January 9, 2018

Microsemi has teamed up with Digi-Key Electronics, a global electronic components distributor, to provide the SmartFusion™2 system-on-chip (SoC) field programmable gate array (FPGA) maker board exclusively to Digi-Key's global customer base. This low-cost evaluation platform lowers the barrier for hardware and firmware engineers to develop embedded applications for the ARM Cortex™-M3 and 12K logic elements (LE) FPGA fabric in the SmartFusion2 device. Contents include the new SmartFusion2 board, a USB cable to provide power, programming and communication, and a QuickStart Guide.

The board is an ideal platform to jumpstart designs using the Microsemi SmartFusion2 SoC FPGA. This device family offers more resources in low density FPGAs all while delivering the lowest power, proven security and single event upset (SEU) FPGA configuration immunity. The key features of the SmartFusion2-010 SoC FPGA are an ARM Cortex-M3 processor, GigE MAC, USB OTG, built in DDR2/3 controller, numerous other peripherals, 12K FPGA LEs and the highest levels of security to protect customers' IP. The board also features a 1000BASE-T PHY and connector, two unpopulated interfaces for the ESP32 and the ESP8266 (not included), USB connectivity and more.

"Microsemi is excited to work with Digi-Key in offering the SmartFusion2 maker board. We believe Digi-Key's broad customer base will benefit from this low-cost platform for a wide variety of applications," said Phil Sansone, vice president of global distribution sales at Microsemi.

The board is the lowest cost evaluation board which enables firmware and design engineers to leverage the power of Microsemi's SmartFusion2 architecture. The board itself is ideal to prototype applications such as internet of things gateway, medical instruments, hand held industrial/test products, motor control, secure connectivity designs, etc.

The SmartFusion2 maker board (M2S010-MKR-KIT) includes the following features:

  • The SmartFusion2 M2S010 SoC FPGA
  • The 10/100/1000BASE-T VSC8541 PHY
  • Wurth Electronics RJ45 7499111221A
  • Ambient light sensor
  • 16 Mbit SPI Flash
  • Eight user LEDs
  • USB integrated FlashPro5 programming hardware
  • Connector for ESP8266 (not included)
  • Laid out footprint for ESP32 (not included)
  • USB port for UART communications
  • LX7167A powering the board
  • 50 MHz clock source
  • 2 user pushbuttons

"This new SmartFusion2 evaluation board is an excellent fit for the greater engineering community," said David Stein, VP, Global Semiconductor at Digi-Key. "It's a powerful, versatile, integrated platform, all at a great value for anyone looking for an introduction to a SmartFusion2 system with Wi-Fi and Ethernet. Digi-Key is pleased to support Microsemi's launch of this low-cost board as it offers our customers a new valuable evaluation platform in FPGA development."

For more information about the Digi-Key SmartFusion2 Maker Board, including user's guides, tutorials, and design examples, or to view Microsemi's entire product listing, visit the Digi-Key website.

About Digi-Key Electronics

Digi-Key Electronics, headquartered in Thief River Falls, Minn., USA, is an authorized global, full-service distributor of electronic components, offering more than six million products, with over 1.3 million in stock and available for immediate shipment, from over 650 quality name-brand manufacturers. Digi-Key also offers a wide variety of online resources such as EDA and design tools, datasheets, reference designs, instructional articles and videos, multimedia libraries, and much more. Technical support is available 24/7 via email, phone and webchat. Additional information and access to Digi-Key's broad product offering can be found by visiting www.digikey.com.