TRIPP'LITE 553
16
Regulatory Compliance & Product Registration
UL CLASSIFICATION FOR MEDICAL EQUIPMENT: Class I, Type B, Ordinary Equipment, Continuous Operation.
UL1778 APPROVAL: All the UPS systems described in this manual are UL1778 listed. All meet strict requirements for UPS protection. They provide battery
backup during blackouts, switching between utility power and battery backup power in 2-4 milliseconds. In addition, all have hospital-grade plugs and
receptacles that reduce the possibility of accidental equipment disconnection. All are suitable for use in hospitals, outside patient care areas.
UL60601-1 APPROVAL: Several of the UPS models described in this manual are UL 60601-1 listed (see specifications). They incorporate Faraday-shielded
isolation transformers that reduce the cumulative leakage current of all connected equipment to below 100 microamps. These models are suitable for use in
hospitals, including inside patient care areas.
REGULATORY COMPLIANCE IDENTIFICATION NUMBERS:
For the purpose of regulatory compliance certifications and identification, your Tripp Lite product has been assigned a unique series number. The series number
can be found on the product nameplate label, along with all required approval markings and information. When requesting compliance information for this
product, always refer to the series number. The series number should not be confused with the marketing name or model number of the product.
FCC Notice, Class A
This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions: (1) This device may not cause harmful interference, and
(2) this device must accept any interference received, including interference that may cause undesired operation.
Note: This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to part 15 of the FCC Rules. These limits
are designed to provide reasonable protection against harmful interference when the equipment is operated in a commercial environment. This equipment
generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful
interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful interference in which case the user will be
required to correct the interference at his own expense. The user must use shielded cables and connectors with this equipment. Any changes or modifications to
this equipment not expressly approved by Tripp Lite could void the user’s authority to operate this equipment.
FCC Notice, Class B
This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions: (1) This device may not cause harmful interference, and
(2) this device must accept any interference received, including interference that may cause undesired operation.
Note: This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits
are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio
frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is
no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which
can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:
• Reorient or relocate the receiving antenna.
• Increase the separation between the equipment and receiver.
• Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.
• Consult the dealer or an experienced radio/TV technician for help.
Any changes or modifications to this equipment not expressly approved by Tripp Lite could void the user’s authority to operate this equipment.
FCC Part 68 Notice (United States Only)
If your Modem/Fax Protection causes harm to the telephone network, the telephone company may temporarily discontinue your service. If possible,
they will notify you in advance. If advance notice isn’t practical, you will be notified as soon as possible. You will be advised of your right to file a complaint
with the FCC. Your telephone company may make changes in its facilities, equipment, operations or procedures that could affect the proper operation of
your equipment. If it does, you will be given advance notice to give you an opportunity to maintain uninterrupted service. If you experience trouble with this
equipment’s Modem/Fax Protection, please visit www.tripplite.com/support for repair/warranty information. The telephone company may ask you to disconnect
this equipment from the network until the problem has been corrected or you are sure the equipment is not malfunctioning. There are no repairs that can be
made by the customer to the Modem/Fax Protection. This equipment may not be used on coin service provided by the telephone company. Connection to party
lines is subject to state tariffs. (Contact your state public utility commission or corporation commission for information.)
EQUIPMENT ATTACHMENT LIMITATIONS (MODELS WITH THE INDUSTRY CANADA LABEL IN CANADA ONLY):
Notice: The Industry Canada label identifies certified equipment. This certification means that the equipment meets the telecommunications network protective,
operational and safety requirements as prescribed in the appropriate Terminal Equipment Technical Requirements Document(s). The Department does not
guarantee the equipment will operate to the user’s satisfaction.
Before installing this equipment, users should ensure that it is permissible to be connected to the facilities of the local telecommunications company.
The equipment must also be installed using an acceptable method of connection. The customer should be aware that the compliance with the above conditions
might not prevent degradation of service in some situations.
Repairs to certified equipment should be coordinated by a representative designated by the supplier. Any repairs or alterations made by the user
to this equipment, or equipment malfunctions, may give the telecommunications company cause to request the user to disconnect the equipment.
Users should ensure for their own protection that the electrical ground connections of the power utility, telephone lines and internal metallic water pipe system,
if present, are connected together. This precaution may be particularly important in rural areas. Caution: Users should not attempt to make connections
themselves, but should contact the appropriate electric inspection authority, or electrician, as appropriate.
PRODUCT REGISTRATION
Visit www.tripplite.com/warranty today to register your new Tripp Lite product. You’ll be automatically
entered into a drawing for a chance to win a FREE Tripp Lite product!*
* No purchase necessary. Void where prohibited. Some restrictions apply. See website for details.
Tripp Lite has a policy of continuous improvement. Product specifications are subject to change without notice.
1111 W. 35th Street, Chicago, IL 60609 USA • www.tripplite.com/support
Note on Labeling
Two symbols are used on the label.
V~ : AC Voltage
V : DC Voltage
17-02-075-933606.indb 16 2/6/2017 11:13:49 AM