XS26-2,SC26-2 Controllers Datasheet by Banner Engineering Corporation

BANNER more sensors, more solutions 00 00 00 00 Expansion Pen Micro USB Pen mug
Datasheet
Important: For complete technical information about this product, including installation instructions, application requirements
and guidelines, technical specifications, and accessories, go to www.bannerengineering.com and search for the instruction
manual, p/n 174868.
Program in minutes with intuitive, easy-to-use configuration software
Up to eight expansion I/O modules can be added as automation requirements grow or
change
Choose from six expansion module models
Expansion module models have a variety of safety inputs, solid-state safety outputs and
safety relay outputs
Innovative live display feature and diagnostics allow for active monitoring of I/O on a PC
and assist in troubleshooting and commissioning
Safety Controller and input modules allow safety inputs to be converted to status outputs
for efficient terminal use
Ethernet-enabled models can be configured for up to 256 virtual status outputs
Optional SC-XM2/3 external drive for fast swap and quick configuration without a PC
Model Features
XS26-2 Expandable
XS26-2d Expandable + Display
XS26-2e Expandable + Ethernet
XS26-2de Expandable + Display + Ethernet
SC26-2 Non-Expandable
SC26-2d Non-Expandable + Display
SC26-2e Non-Expandable + Ethernet
SC26-2de Non-Expandable + Display + Ethernet
Note: Configuration software is required.
The software is available at http://www.bannerengineering.com/safetycontroller.
Features Diagram
Ethernet Port
Indicator LED’s
Onboard Interface Push Buttons
Onboard Display
Wiring Terminals
Expansion Port
Micro USB Port
Wiring Terminal
Row Designation
Responsibilities of Qualified Personnel
To access the Banner Safety Controller instruction manual (p/n 174868 ):
Go to www.bannerengineering.com to download the manual in the language you require; or
Call Banner at 1-888-373-6767 or call your local Banner Representative to request a manual
WARNING:
It is the responsibility of the Qualified Personnel to:
Carefully read, understand, and follow the information in the XS/SC26-2 instruction manual
Perform a risk assessment of the specific machine guarding application
Determine what risk reduction measures are appropriate per the results of the risk assessment
Properly install, configure, and then verify that the risk reduction measures are working as intended
Periodically re-verify, as needed, that the risk reduction measures are working as intended
Failure to follow any of these responsibilities may potentially create a dangerous condition that could lead to serious injury or
death.
XS26-2/SC26-2 Base Safety Controllers
Original Document
175119 Rev. L 10 August 2020
175119
BANNER more 34211505,“er solutions
Pour accéder au manuel d'utilisation Banner Safety Controller (réf. 174868 ):
Rendez-vous sur le site www.bannerengineering.com pour télécharger le manuel dans la langue de votre choix, ou
Contactez Banner au 1-888-373-6767 ou appelez votre représentant Banner local pour demander le manuel.
WARNING:
Il incombe au personnel qualifié de:
Lire avec attention, bien comprendre et suivre les instructions du manuel du système XS/SC26-2
Effectuer une évaluation des risques de l'application de protection spécifique à la machine
Identifier les mesures de limitation du risque appropriées en fonction des résultats de l'étude de risques
Installer et configurer correctement le ou les dispositifs de protection destinés à limiter le risque puis vérifier qu’ils
fonctionnent de la façon prévue
Revérifier périodiquement, s'il y a lieu, que ces dispositifs de protection fonctionnent toujours comme il se doit
Le non-respect de l'une de ces responsabilités peut potentiellement créer une condition dangereuse pouvant entraîner des
blessures graves, voire mortelles.
So beziehen Sie die Bedienungsanleitung für den Banner Safety Controller (Ident-Nr. 174868 ):
Laden Sie die Anleitung in der gewünschten Sprache von unserer Website (www.bannerengineering.com) herunter oder
fordern Sie die Anleitung telefonisch bei der Banner-Hotline unter der Rufnummer +1-888-373-6767 oder bei einer Banner-Vertretung in
Ihrer Nähe an.
WARNING:
Es liegt in der Verantwortung des qualifizierten Personals,
Die Informationen in der Anleitung für den XS/SC26-2 gründlich durchzulesen, zu verstehen und zu befolgen
Eine Risikobeurteilung der spezifischen Maschinenschutzanwendung durchzuführen
Ermitteln, welche Maßnahmen zur Risikominderung aufgrund der Ergebnisse der Risikobeurteilung angemessen sind
Das gesamte Schutzsystem fachgerecht installieren, konfigurieren und anschließend auf die bestimmungsgemäße
Funktion überprüfen
Je nach Bedarf regelmäßig nachprüfen, ob die Maßnahmen zur Risikominderung wie beabsichtigt funktionieren
Die Nichtbeachtung einer dieser Verantwortlichkeiten kann zu gefährlichen Zuständen führen, die zu schweren oder tödlichen
Verletzungen führen können.
Per accedere al manuale di istruzioni dello Banner Safety Controller (codice 174868 ):
Andare al sito www.bannerengineering.com per scaricare il manuale nella lingua desiderata; oppure
Contattare Banner al numero telefonico 1-888-373-6767 oppure il rappresentante Banner locale per richiedere un manuale
WARNING:
È responsabilità della Personale Qualificato:
Leggere attentamente, assicurarsi di avere compreso e seguire le indicazioni riportate nel manuale di istruzioni del
XS/SC26-2
Eseguire una valutazione dei rischi dell'applicazione di protezione della macchina specifica
Determinare quali misure di riduzione del rischio sono appropriate in base ai risultati della valutazione del rischio
Installare e configurare correttamente il sistema, quindi verificare che le misure di riduzione del rischio assicurino i
risultati previsti
Ricontrollare periodicamente, in base alla necessità, che tali misure di riduzione del rischi continuino ad assicurare i
risultati previsti
La mancata osservanza di una qualsiasi di queste responsabilità può potenzialmente creare una condizione pericolosa che
potrebbe causare lesioni gravi o mortali.
Para obtener el manual de instrucciones del Banner Safety Controller (p/n 174868 ):
Visite www.bannerengineering.com para descargar el manual en el idioma que necesite; o
Llame a Banner al 1-888-373-6767 o llame a su representante local de Banner para solicitar un manual
WARNING:
Es responsabilidad del personal calificado:
Leer con atención, entender y seguir la información en el manual de instrucciones de la XS/SC26-2
Realizar una evaluación de riesgos que incluya la aplicación de protección de la máquina específica
Determinar qué medidas de reducción de riesgos son apropiadas según los resultados de la evaluación de riesgos
Instale, configure y luego verifique correctamente que las medidas de reducción de riesgos funcionan según lo
previsto
Vuelva a verificar periódicamente, según sea necesario, que las medidas de reducción de riesgos funcionan según lo
previsto
El incumplimiento de cualquiera de estas responsabilidades puede crear potencialmente una condición peligrosa que podría
provocar lesiones graves o la muerte.
Banner Engineering Corp. Limited Warranty
Banner Engineering Corp. warrants its products to be free from defects in material and workmanship for one year following the date of shipment. Banner Engineering Corp. will repair or replace, free of charge,
any product of its manufacture which, at the time it is returned to the factory, is found to have been defective during the warranty period. This warranty does not cover damage or liability for misuse, abuse, or the
improper application or installation of the Banner product.
THIS LIMITED WARRANTY IS EXCLUSIVE AND IN LIEU OF ALL OTHER WARRANTIES WHETHER EXPRESS OR IMPLIED (INCLUDING, WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY OR
FITNESS FOR A PARTICULAR PURPOSE), AND WHETHER ARISING UNDER COURSE OF PERFORMANCE, COURSE OF DEALING OR TRADE USAGE.
This Warranty is exclusive and limited to repair or, at the discretion of Banner Engineering Corp., replacement. IN NO EVENT SHALL BANNER ENGINEERING CORP. BE LIABLE TO BUYER OR ANY OTHER
PERSON OR ENTITY FOR ANY EXTRA COSTS, EXPENSES, LOSSES, LOSS OF PROFITS, OR ANY INCIDENTAL, CONSEQUENTIAL OR SPECIAL DAMAGES RESULTING FROM ANY PRODUCT DEFECT OR
FROM THE USE OR INABILITY TO USE THE PRODUCT, WHETHER ARISING IN CONTRACT OR WARRANTY, STATUTE, TORT, STRICT LIABILITY, NEGLIGENCE, OR OTHERWISE.
Banner Engineering Corp. reserves the right to change, modify or improve the design of the product without assuming any obligations or liabilities relating to any product previously manufactured by Banner
Engineering Corp. Any misuse, abuse, or improper application or installation of this product or use of the product for personal protection applications when the product is identified as not intended for such
purposes will void the product warranty. Any modifications to this product without prior express approval by Banner Engineering Corp will void the product warranties. All specifications published in this
document are subject to change; Banner reserves the right to modify product specifications or update documentation at any time. Specifications and product information in English supersede that which is
provided in any other language. For the most recent version of any documentation, refer to: www.bannerengineering.com.
For patent information, see www.bannerengineering.com/patents.
XS26-2/SC26-2 Base Safety Controllers
© Banner Engineering Corp. All rights reserved