Home 14. Hooking up ground cords.
TB-2000 Page 4 of 4
Figure 14. Hooking up ground cords.
4. If your installation includes a floor mat, you should duplicate
step 2 and attach the floor mat ground to the same point as the
worksurface ground wire.
5. Measure the resistance from the ground snap on the mat to
the common ground point. It should read 1 megohm ± 20
percent if you are using a ground cord with a resistor, and less
than 1 ohm if you are using a non-resistor ground cord.
6. Using a surface resistance tester per ESD TR53, test the
resistance to ground from the center of the mat surface.
Required equipment: a megohmmeter with 100 volt open test
circuit voltage and two five pound electrodes per ASTM-150.
Desco sells this as the Digital Surface Resistance Meter
Kit, item 19787. For more information on the 19787, ask for
Technical Bulletin TB-3062.
Limited Warranty, Warranty Exclusions, Limit of Liability
and RMA Request Instructions
See Desco’s Terms and Conditions -
http://desco.descoindustries.com/TermsAndConditions.aspx
DESCO WEST - 3651 Walnut Avenue, Chino, CA 91710 • (909) 627-8178
DESCO EAST - One Colgate Way, Canton, MA 02021-1407 • (781) 821-8370 • Web Site: Desco.com
Figure 13. Installing 09814 to mat using supplied hardware.
Mat Installation - General Information
1. For best results, allow the mats to lay flat for about four
hours at room temperature before installing. This will give the
material time to flatten out from being rolled for shipment.
2. Test grounds for proper resistance to ground. See Desco
Technical Bulletin TB-2007 for a complete discussion of
grounds.
3. Lay the mat in position and snap the ground cord to it. Bring
the other end of the ground cord to the common ground point
and attach it using the ring terminal. A suggested ground point
is the center screw of a standard AC electrical outlet. Testing is
recommended to ensure that the screw is properly grounded.
Tie the ground wire to the bench to keep it out of the way and
neat. You may cut and strip the ground wire to a shorter length
and attach it with the extra ring terminal included with each
Desco ground cord.
Figure 15. Adding the wriststrap.
BE SURE YOU TEST ALL GROUNDS AND THE WRIST STRAP
FREQUENTLY.
The following bulletins are available from Desco:
TB-2004 Operation of 19350 Wrist Strap Tester
TB-2005 Wrist Straps, Grounding, Testing, Maintenance
TB-2007 Safe Grounding of Static Controlled Workstations
Maintenance and Cleaning
For optimum performance, periodic cleaning is required following
manufacturer’s recommendations. Desco recommends Reztore™
Surface and Mat Cleaner for workstation mats and other surfaces
and Statguard® Floor Mat Cleaner for floor mats.
Note: Desco’s Reztore™ Surface and Statguard® Floor Mat
Cleaners contain no silicone or harsh solvents. Cleaners with
silicone leave an insulative residue on surfaces and solvents such
as 2-Butoxyethanol or Ethanolamine used in cleaners can dry out
the material; both can prevent conductive or dissipative mats from
functioning properly.
09825 / 09826
“GREEN WIRE”
UTILITY
GROUND
POINTS
RING
TERMINAL
CAN BE
ATTACHED
HERE
© 2015 DESCO INDUSTRIES INC.
Employee Owned
7. If you are using a mat kit that includes the wrist strap, install
the wrist strap directly to the common point mat ground cord
banana jack. Again, test the resistance from the backplate of
the wrist strap to the common ground point. It should read 1
Megohm ± 20 percent.
6. The 09813 / 09814 mat ground cord may be either attached to
a mat by snapping onto a 10mm socket, or by bolting it to the
mat with the hardware supplied with the cord. When bolting
the 09814 to the mat use a 3/8" diameter hole punch to create
the hole for mounting. This will allow cord to sit flush on the
mat. Note: For both applications, remove screw from floor mat
ground before attaching to mat.