HHR75AAA/B Datasheet

Panasonic - BSG

View All Related Products | Download PDF Datasheet

Datasheet


 
2
3


We are able to offer you a wide range of individual power
solu tions for portable and stationary applications. Our prod uct
range includes high reliability batteries such as Lithium-Ion,
Lithium, Nickel-Metal-Hy dride, Valve-Regu lated-Lead-Acid
(VRLA), Alkaline and Zinc-Carbon. Based on this battery
range we can power your busi ness in virtually all applications.

Panasonic Energy Company (PEC) started its battery produc-
tion
in 1931. Today PEC is the most diversified global battery
manu facturer with a network of 16 manufacturing companies
in 14 countries. More than 12,600 employees are dedicated
to the research & development and in the production of new
batteries for a new world.
When it comes to production our facilities employ leading
edge manufacturing processes meeting the highest quality
standards. Our factories are certified to ISO standards. This
means that each factory has its own quality and environ-
mental management. The ISO 9000 and ISO 14000 series are
the minimum benchmarks that ensure our excellent product
reliability.
Furthermore the majority of our factories is also certified to
OHSAS 18001 (Occupational Health and Safety Assessment
Series), an international standard for assessing a manage-
ment system for occupational safety. This confirms that our
factories have been proactive in putting the occupational
health and safety of its staff at the centre of the com pany‘s
dealings. In addition our VRLA batteries are for example
approved to German VdS standard and U.S. UL standard.
Panasonic quality
certified by authorised companies.

Panasonic Corporation, foun ded in Osaka 1918, is one of the world’s largest manufacturers of
quality electronic and electrical equipment. Its subsidiary, Panasonic Industrial Europe GmbH
(PIE) deals with a wide diversified range of in dus trial products for all European countries.
This company was formed in 1998 to strengthen Panasonic’s Pan-European industry operation,
and today is active in such different business fields as Automotive, Audio/Video & Communication,
Appliance and Industry & Devices to satisfy its customer’s needs.
Audio/Video &
Communication
PMG (Product
Marketing Group)
Industry & Devices
Automotive
Appliance
Factory Solutions
5


Pursuing coexistence with the global environment in its business vision, Panasonic places
reduction of the environmental impact in all its business activities as one of the important
themes in its mid-term management plan. In its ‘eco ideasStrategy, which focuses in particular
on rapid implementation of measures to prevent global warming and global promotion of envi-
ronmental sustainability management, Panasonic is advancing three key initiatives: ‘eco ideas
for Manufacturing, ‘eco ideasfor Products, and ‘eco ideasfor Everybody, Everywhere.

We are approaching a global turning
corner and it would not be an ex ag-
geration to call it the ‘Environmental
Industrial Revolution’. Based on this
rec og nition, Panasonic has built an
‘eco ideas’ House on the premise of our
showroom, Panasonic Center Tokyo in
April 2009 in order to help create a
carbon-free society and reduce CO2
emissions from a household sector.
The concept of this ‘eco ideas’ House
can be described as follows:
1. Virtually zero CO2 emissions in an
entire house envisaged in three to
five years into the future
2. Synergy of technology and nature
Aforementioned concepts shows that
Panasonic is not only aware of is en vi -
ron mental responsibility moreover
this Panasonic takes action.

We will reduce CO2 emissions across all
our manufacturing sites.

In each of our factories a CO
2
emissions
of 10% reduction till 2010.

Our factories are evaluated with regard to
CO2 emission, waste disposal, recycling
measures as well as chemical and water
consumption within the scope of the
‘Clean Factory’ program and they are set
performance targets according to these
indicators.

The Wakayama Plant of the Energy Com-
pany is strengthening its management
structure to cut CO2 emissions from the
main production bases for Lithium-Ion
batteries, which are a core component of
Panasonic’s energy business. As a result,
it has succeeded in roughly halving CO2
emissions per production unit, as well as
sharply curbing an increase in CO2 emis-
sions even as production has expanded.

We will produce energy-efficient pro-
ducts.

In March 2010 at least 20 products with
the ‘Superior Green Products‘ classifi-
cation should be available.

The developers at Panasonic carry out
an environmental impact assessment
for all our products. Products that meet
the highest environmental requirements
in the branch with regard to conservation
of energy and energy efficiency are
classified as a ‘Superior Green Product’
and awarded the Panasonic logo ‘eco
ideas’.

We have dispensed with the use of
highly toxic Lithium Thionyl Chloride in
the production of our Lithium batteries.
This is quite rightly classified as highly
toxic and should never under any cir-
cumstances be released into the envi-
ronment.

We will encourage the spread of environ-
mental activities throughout the world.

Intensive commitment on the part of the
company owners, international coopera-
tions and involvement of the employees.

Not only do we sponsor the work of the
WWF for the Arctic, Panasonic has also
launched a couple of other environmen-
tal
initiatives such as the ECO RELAY ini-
tiative in which hundreds of colleagues
the world over take part voluntarily for
several days in environmental campaigns.

With the support of the GRS Batterien
(German
Battery Recycling Association)
Panasonic arranged a battery collection
day with the aim of collecting as many of
these spent energy sources as possible
and giving out information about
the
recycling loop of batteries from which
valuable raw materials such as Zinc,
Manganese and Iron can be recovered.







4
66
77

Chapter Page
 
Charging 7
Discharging 7
Storage 8
Service life of batteries 8
Design of products which use batteries 8 – 9
Prohibited items regarding the battery handling 9 – 10
Other precautions 10
Ni-MH battery transportation situation 10
Final point to keep in mind 10
  11
 
Overview 12
Construction 12
Applications 12
Structure of Ni-MH batteries 13
The principle of electrochemical reaction involved in Ni-MH batteries 13 – 14
Features 14
Five main characteristics 14 – 16
 
Charge methods 17 – 18
Ni-MH high-temperature series recommended charge for back-up power applications 18
  19
 fi 20
  21 – 44
  45
  46 – 47
In order to take full advantage of the properties of Ni-MH
batteries and also to prevent problems due to improper use,
please note the following points during the use and design of
battery operated products.


Charge batteries within an ambient temperature range of
C to 4C. Ambient temperature during charging affects
charging efficiency. As charging efficiency is best within a
temperature range of 10°C to 30°C, whenever possible place
the charger (battery pack) in a location within this tempera-
ture range.
At temperatures below C the gas absorption reaction is
not adequate, causing gas pressure inside the battery to rise,
which can activate the safety vent and lead to leakage of
alkaline gas and deterioration in battery performance.
Charging efficiency drops at temperatures above 40°C. This
can disrupt full charging and lead to deterioration in perform-
ance and battery leakage.

Sufficient care must be taken during the design of the
charger when charging batteries connected in parallel.
Consult Panasonic when parallel charging is required.

Never attempt reverse charging. Charging with polarity
reversed can cause a reversal in battery polarity causing gas
pressure inside the battery to rise, which can activate the safety
vent, lead to alkaline electrolyte leakage, rapid deterioration
in
battery performance, battery swelling or battery rupture.

Avoid overcharging. Repeated overcharging can lead to
deterioration in battery performance. (‘Overcharging’ means
charging a battery when it is already fully charged.)

To charge batteries rapidly, use the specified charger (or
charging method recommended by Panasonic) and follow the
correct procedures.

Trickle charging cannot be used with Ni-MH batteries, except
specific high temperature batteries (please contact Panasonic
to get more information). However, after applying a refresh
charge using a rapid charge, use a trickle charge of 0.033CmA
to 0.05CmA. Also, to avoid overcharging with trickle charge,
which could damage the cell characteristics, a timer meas-
uring the total charge time should be used.

During charging and discharging, ‘CmAis a value indicating
current and expressed as a multiple of nominal capacity.
Substitute ‘C’ with the batterys nominal capacity when calcu-
lating. For example, for a 1500mAh battery of 0.033CmA, this
value is equal to 1/30 x 1500, or roughly 50mA.


Discharge batteries within an ambient temperature range of
-10°C to +45°C.
Discharge current level (i. e. the current at which a battery is
discharged) affects discharging efficiency. Discharging
effi-
ciency is good within a current rangeof 0.1CmA to 2CmA.
Discharge capacity drops at temperatures below -10°C or
above +4C. Such decreases in discharge capacity can lead
to deterioration in battery performance.

Since overdischarging (deep discharge) damages the battery
characteristics, do not forget to turn off the switch when
discharging, and do not leave the battery connected to the
equipment for long periods of time. Also, avoid shipping the
battery installed in the equipment.

As high-current discharging can lead to heat generation and
decreased discharging efficiency, consult Panasonic before
attempting continuous discharging or pulse discharging at
currents larger than 2CmA.
88
99



Store batteries in a dry location with low humidity, no corro-
sive gases, and at a temperature range of -2C to +4C.
Storing batteries in a location where humidity is extremely
high or where temperatures fall below -20°C or rise above
+45°C can lead to the rusting of metallic parts and battery
leakage due to expansion or contraction in parts composed
of organic materials.

Because long-term storage can accelerate battery self-
discharge and lead to the deactivation of reactants, locations
where the temperature ranges between +10°C and +30°C are
suitable for long-term storage.
When charging for the first time after long-term storage,
deactivation of reactants may lead to increased battery voltage
and decreased battery capacity. Restore such batteries to
original performance by repeating several cycles of charging
and discharging.
When storing batteries for more than 1 year, charge at least
once a year to prevent leakage and deterioration in perform-
ance due to selfdischarging.


Batteries used under proper conditions of charging and
discharging can be used 500 cycles or more. Significantly
reduced service time in spite of proper charging means that
the life of the battery has been exceeded.
Also, at the end of service life, an increase in internal resist-
ance, or an internal short-circuit failure may occur. Chargers
and charging circuits should therefore be designed to ensure
safety in the event of heat generated upon battery failure at
the end of service life.

Because batteries are chemical products involving internal
chemical reactions, performance deteriorates not only with
use but also during prolonged storage.
Normally, a battery will last 2 years (or 500 cycles) if used
under proper conditions and not overcharged or overdis-
charged. However, failure to satisfy conditions concerning
charging, discharging, temperature and other factors during
actual use can lead to shortened life (or cycle life) damage to
products and deterioration in performance due to leakage and
shortened service life.


Never solder a lead wire and other connecting materials
directly to the battery, as doing so will damage the batterys
internal safety vent, separator, and other parts made of
organic materials. To connect a battery to a product, spot-
weld a tab made of nickel or nickel-plated steel to the
batterys terminal strip, then solder a lead wire to the tab.
Perform soldering in as short a time as possible.
Use caution in applying pressure to the terminals in cases
where the battery pack can be separated from the equip-
ment.

Because small amounts of alkaline electrolyte can leak from
the battery seal during extended use or when the safety vent
is activated during improper use, a highly alkaline-resistant
material should be used for a product’s contact terminals in
order to avoid problems due to corrosion.
(Note that stainless steel generally results in higher contact resistance.)

Excessively high temperatures (i.e. higher than 4C) can
cause alkaline electrolyte to leak from the battery, thus
damaging the product and shorten battery life by causing
deterioration in the separator or other battery parts. Install
batteries far from heat-generating parts of the product. The
best battery position is in a battery compartment that is
composed of an alkaline-resistant material which isolates
the batteries from the product’s circuitry. This prevents
damage that may be caused by a slight leakage of alkaline
electrolyte from the battery.

The discharge end voltage is determined by the formula given
below. Please set the end voltage of each battery at 1.1 volts
or less.

Overdischarging (deep discharging) or reverse charging
damages the battery characteristics. In order to prevent
damage associated with forgetting to turn off the switch or
leaving the battery in the equipment for extended periods,
preventative options should be incorporated in the equip-
ment. At the same time, it is recommended that leakage
current is minimized. Also, the battery should not be shipped
inside the equipment.


Panasonic assumes no responsibility for problems resulting
from batteries handled in the following manner.

Never disassemble a battery, as the electrolyte inside is
strong alkaline and can damage skin and clothes.

Never attempt to short-circuit a battery. Doing so can damage
the product and generate heat that can cause burns.

Disposing of a battery in fire can cause the battery to rupture.
Also avoid placing batteries in water, as this causes batteries
to cease to function.

Never solder anything directly to a battery. This can destroy
the safety features of the battery by damaging the safety vent
inside the cap.

Never insert a battery with the positive and negative poles
reversed as this can cause the battery to swell or rupture.

Never reverse charge or overcharge with high currents (i.e.
higher than rated). Doing so causes rapid gas generation and
increased gas pressure, thus causing batteries to swell or
rupture.
Charging with an unspecified charger or specified charger
that has been modified can cause batteries to swell or
rupture. Be sure to indicate this safety warning clearly in all
operating instructions as a handling restriction for ensuring
safety.


Always avoid designing airtight battery compartments. In
some cases, gases (oxygen, hydrogen) may be given off, and
there is a danger of the batteries bursting or rupturing in the
presence of a source of ignition (sparks generated by a motor
switch, etc.).

Do not use a battery in an appliance or purpose for which it
was not intended. Differences in specifications can damage
the battery or appliance.
 
Nickel, stainless steel, nickel-plated
steel, etc.
Tin, aluminum, zinc, copper, brass,
etc.

1 to 6 (Number of batteries x 1.0) V
7 to 12 (Number of batteries - 1) x 1.2) V
1010
1111


Special caution is required to prevent short circuits. Care
must be taken during the design of the battery pack shape to
ensure batteries cannot be inserted in reverse. Also, caution
must be given to certain structures or product terminal
shapes which can make short-circuiting more likely.

Avoid using old and new batteries together. Also avoid
using
these batteries with ordinary dry-cell batteries,
Ni-Cd batteries or with another manufacturers batteries.
Differences in various characteristic values, etc., can cause
damage to batteries or the product.

Batteries should always be charged prior to use. Be sure to
charge correctly.



Ni-MH batteries are classified as no dangerous goods under
IMDG-Code 34-08 (International Maritime Dangerous Goods
Code), vaild until 31.12.2011.
From 01.01.2012 new UN 3496 takes place under IMDG-Code
35-10 with Special Provision 963. Ni-MH batteries are then
classified as dangerous goods in class 9. Batteries shall be
securely packed and protected from short circuit.
When loaded in a cargo transport unit with 100kg gross
mass or more, special stowage is requested away from heat
source. Furthermore an information on the IMO (International
Maritime Organization) document is required.

As of today there are no fixed regulations for the worldwide
transportation of Ni-MH batteries by air.

As of today there are no fixed regulations for the worldwide
transportation of Ni-MH batteries by road.

In order to ensure safe battery use and to prolong the battery
performance, please consult Panasonic regarding charge
and discharge conditions for use and product design prior to
the release of a battery-operated product.
*1 The aforementioned information is subject to change without any notice.


Name of Company: Panasonic Corporation Energy Company
Address: 1-1, Matsushita-cho, Moriguchi, Osaka 570-8511 Japan
Document number: PMH-PSDS-100129E
Issued: Jan, 29th , 2010
Name of product: Nickel-Metal-Hydride Storage Battery
(Model Name) The models described as HHR-*****

Substance: Nickel-Metal-Hydride Storage Battery
CAS No.: Not Specified.
UN Class: Classified as UN3028, but they are exempted from Dangerous Goods pursuant to UN
Special Provision as below. Not restricted, as per Special Provision A123
[Special Provision 304] (UN Recommendations on the TRANSPORT OF DANGEROUS GOODS Model Regulations
Volume 1. 15th revised edition) Battery, dry, containing corrosive electrolyte which will not flow out of the
battery if the battery case is cracked are not subject to these Regulations provided the batteries are securely
packed and protected against short-circuits. Examples of such batteries are: Alkali-Manganese, Zinc-Carbon,
Nickel-Metal-Hy dride and Nickel-Cadmium batteries.

Heavy metal quantity for cell: Hg < 0.5ppm Measurement Analysis: Atomic Absorption Spectrometer
Cd < 5.0ppm Measurement Analysis: Atomic Absorption Spectrometer
Pb < 40ppm Measurement Analysis: Atomic Absorption Spectrometer

1. During the transportation of a large amount of batteries by ship, trailer or railway, do not leave them in the
places of high temperatures and do not allow them to be exposed to dew condensation.
2. Avoid transportation with the possibility of the collapse of cargo piles and the packing damage.
3.
Protect the terminals of batteries and prevent them from short circuit so as not to cause dangerous heat
generation.

- IATA Dangerous Goods Regulations 51th Edition Effective 1 January 31 December 2010
- ICAO Technical Instructions for the safe transport of dangerous goods by air
- IATA (A123) for air shipment and IMDG (Special Provision) for sea shipment under UN3028


- Ni-Cd, Ni-MH Panasonic Catalogue and technical handbook.
- MSDS of Nickel hydro oxide and potassium hydro oxide and sodium hydro oxide from supplier.
- Recommendations on the TRANSPORT OF DANGEROUS GOODS Model Regulations Volume 1. 15
th
revised edition.
- IATA Dangerous Goods Regulations 51th Edition Effective 1 January – 31 December 2010
- Technical Instructions for the Safe Transport of Dangerous Goods by Air
(Approved and published by decision of the Council of ICAO) 2003-2004 Edition

*1 The aforementioned PSDS is only an extract. Please contact Panasonic to get the complete version.
1212
1313

More and more electric products with sophisticated func-
tions require extremely compact and light battery solutions
delivering a high level of energy density. To meet these
needs Panasonic Ni-MH batteries have been developed and
manufactured with nickel hydroxide for the positive electrode
and hydrogen-absorbing alloys, capable of absorbing and
releasing hydrogen at high-density levels, for the negative
electrode. The Ni-MH battery technology is nowadays the Ni-Cd
(nickel cadmium) successor technology for rechargeable and
portable devices. All of our Ni-MH batteries are cadmium-
free, in order not to be harmful to human beings and our
environment.

Ni-MH batteries consist of a positive plate containing nickel
hydroxide as its principal active material, a negative plate
mainly composed of hydrogen-absorbing alloys, a separator
made of fine fibers, an alkaline electrolyte, a metal case and a
sealing plate provided with a self-resealing safety vent. Their
basic structure is identical to that of Ni-Cd batteries. With
cylindrical Ni-MH batteries, the positive and negative plates
are divided by the separator, wound into a coil, inserted into
the case, and sealed by the sealing plate through an electrically
insulated gasket, see page 13.
Panasonic expands the line of Ni-MH cells that are superior
to standard Ni-MH products in applications with low-rate
charge at high temperatures. Improvements were made in
existing Panasonic Ni-MH cells to the negative plate alloy and
separator fiber density. A different electrolyte composition
was achieved to improve performance. Superior long-life
char acteristics can be achieved when combined with appro-
priate intermittent charge control circuitry. The intermittent
charge consumes 1/30th the electricity compared to trickle
charge and more than doubles the expected life of the
Ni-MH
cells compared to Ni-Cd cells that have been trickle
charged.

Panasonic Ni-MH batteries can either be used for standard
applications with a moderate ambient temperature or for
applications which requires high temperature resistance.

E-Bikes, Pedelecs, Scooters, Golf-Trollies, Powertools, Grape-
Cutters, Multimeters, Voting Machine, Barcode Readers,
Hand held Scanners, Labelprinters, Vacuum Cleaners, Muscle
Electro
-Stimulations,
Toothbrushes, etc.

Combined Solar Applications, Portable Medical Devices, POS
Terminals, Emergency Light for buildings and trains, Elevator
Safety Systems, etc.

 Positive pole
 Top plate
 Gasket
 Safety vent
 Collector
 Separator
 Cathode (nickel hydroxide)
 Negative pole (cell can)
 Anode (hydrogen absorbing alloy)
  Insulation plate
  Exhaust gas hole
 Tube






Positive Ni(OH)
2
+ OH- NiOOH + H
2
O + e-
electrode:
Negative M + H
2
O + e- MH
ab
+ OH-
electrode:
Overall Ni(OH)
2
+ M NiOOH + MH
ab
reaction:
(M: hydrogen-absorbing alloy; H
ab
: absorbed hydrogen)
Charge
Discharge
Charge
Discharge
Charge
Discharge



Hydrogen-absorbing alloys have a comparatively short
history which dates back about 20 years to the discovery of
NiFe, MgNi and LaNi5 alloys. They are capable of absorbing
hydrogen equivalent to about a thousand times of their own
volume, generating metal hydrides and also of releasing the
hydrogen that they absorbed. These hydrogen-absorbing
alloys combine metal (A) whose hydrides generate heat
exothermically with metal (B) whose hydrides generate heat
endothermically to produce the suitable binding energy so
that hydrogen can be absorbed and released at or around
normal temperature and pressure levels. Depending on
how metals A and B are combined, the alloys are classified
into the following types: AB (TiFe, etc.), AB2 (ZnMn2, etc.),
AB5 (LaNi5, etc.) and A2B (Mg2Ni, etc.). From the perspective
of charge and discharge efficiency and durability, the field
of candidate metals suited for use as electrodes in storage
batteries is now being narrowed down to AB5 type alloys in
which rare-earth metals, especially metals in the lanthanum
group, and nickel serve as the host metals; and to AB2 type
alloys in which the titanium and nickel serve as the host
metals. Panasonic is now focusing its attention on AB5
type alloys which feature high capacity, excellent charge
and discharge efficiency, and excellent cycle life. It has
developed, and is now employing its own MmNi5 alloy which
uses Mm (misch metal an alloy consisting of a mixture of
rare-earth elements) for metal A.

Ni-MH batteries employ nickel hydroxide for the positive
electrode similar to Ni-Cd batteries. The hydrogen is stored
in a hydrogen-absorbing alloy for the negative electrode,
and an aqueous solution consisting mainly of potassium
hydroxide for the electrolyte. Their charge and discharge
reactions are shown below.
As can be seen by the overall reaction given above, the chief
characteristics of the principle behind a Ni-MH battery is that
hydrogen moves from the positive to the negative electrode
during charge and reverse during discharge, with the elec-
trolyte taking no part in the reaction; which means that there
is no accompanying increase or decrease in the electrolyte.
A model of this batterys charge and discharge mechanism
is shown in the figure on the following page. These are the
useful reactions taking place at the respective boundary
1414
1515
 
faces of the positive and negative electrodes, and to assist
one in understanding the principle, the figure shows
ho
w the
reactions proceed by the transfer of protons (H+).
The hydrogen-absorbing alloy negative electrode success-
fully reduces the gaseous oxygen given off from the positive
electrode during overcharge by sufficiently increasing the
capacity of the negative electrode which is the same method
employed by Ni-Cd batteries.
By keeping the battery’s internal pressure constant in this
manner, it is possible to seal the battery.


These batteries have similar discharge characteristics to
those of Ni-Cd batteries.

Ni-MH batteries have approximately double the capacity
compared with Panasonic’s standard Ni-Cd batteries.

Like Ni-Cd batteries, Ni-MH batteries can be repeatedly
charged and discharged for about 500 cycles. (example: IEC
charge and discharge conditions)

Ni-MH batteries can be rapidly charged in about an hour
using a specially designed charger.

Since the internal resistance of Ni-MH batteries is low,
continuous high-rate discharge up to 3CmA is possible.

As with Ni-Cd batteries, Ni-MH batteries have five main
characteristics: charge, discharge, storage life, cycle life and
safety.

The charge characteristics of Ni-MH batteries are affected
by current, time and temperature. The battery voltage
rises when the charge current is increased or when the
temperature is low. The charge efficiency differs depending
on the current, time, temperature and other factors. Ni-MH
batteries should be charged at a temperature ranging from
C to 40°C using a constant current of 1C or less. The charge
efficiency is particularly good at a temperature of 10°C to
30°C. Repeated charge at high or low temperatures causes
the battery performance to deteriorate. Furthermore, repeated
overcharge should be avoided since it will downgrade the
battery performance. Refer to the section on recommended

charge
methods for details on how to charge the batteries,
see page 17–18.

The discharge characteristics of Ni-MH batteries are
affected by current, temperature, etc., and the discharge
voltage characteristics are flat at 1.2V, which is almost the
same as for Ni-Cd batteries. The discharge voltage and
discharge efficiency decrease in proportion as the current
rises or the temperature drops. As with Ni-Cd batteries,
repeated charge and discharge of these batteries under
high discharge cut-off voltage conditions (more than 1.1V
per cell) causes a drop in the discharge voltage (which
is sometimes accompanied by a simultaneous drop in
capacity). The discharge characteristics can be restored by
charge and discharge to a discharge end voltage of down to
1.0V per cell.





1616
1717
 

These characteristics include self-discharge characteristics
and restoration characteristics after long-term storage.
When batteries are left standing, their capacity generally
drops due to self-discharge, but this is restored by charge.
Self-discharge is affected by the temperature at which the
batteries are left standing and the length of time during
which they are left standing. It increases in proportion
as the temperature or the shelf-standing time increases.
Panasonic’s Ni-MH batteries have excellent self-discharge
characteristics.

The cycle life of these batteries is governed by the conditions
under which they are charged and discharged, temperature
and other conditions of use. Under proper conditions of
use (example: IEC charge and discharge conditions), these
batteries can be charged and discharged for more than 500
cycles.

When the internal pressure of these batteries rises due to
overcharge, short-circuiting, reverse charge or other abuse
or misuse, the self-resealing safety vent is activated to
prevent battery damage.


 
Charge is the process of restoring a discharged battery to
its original capacity. In order for a battery to be usable for a
long period of time, it must be charged via the proper charge
method. Various methods are used to charge recharge-
able cells, but Panasonic recommends the charge methods
described below to charge its Ni-MH batteries.
    1CmA (rapid charge temperature
range: 0°C to 40°C). In order to exercise proper control
to stop rapid charge, it is recommended that batteries be
charged at over 0.5CmA but less than 1CmA. Charging
batteries at a current in excess of 1CmA may cause the safety
vent to be activated by a rise in the internal pressure of the
batteries, thereby resulting in electrolyte leakage. When the
temperature of the batteries is detected by a thermistor or
other type of sensor, and their temperature is under C or
over 40°C at the commencement of the charge, then trickle
charge, rather than rapid charge, must be performed. Rapid
charge is stopped when any one of the values among the
types of control described in (4), (5), (6), and (11) reaches the
prescribed level.
 to flow to excessively discharged or
deep-discharged batteries during charge may make it impos-
sible to sufficiently restore the capacity of the batteries. To
charge excessively discharged or deep-discharged batteries,
first allow a trickle current to flow, and then proceed with the
rapid charge current once the battery voltage has risen.
 Approx. 0.8V/cell rapid charge
transition voltage restoration current: 0.2 ~ 0.3CmA
      Approx. 1.8V/cell.
The charge method is switched over to trickle if the battery
voltage reaches approximately 1.8V/cell due to trouble or
malfunctioning of some kind.
5 to 10mV/cell. When the battery voltage drops
from its peak to 5 to 10mV/cell during rapid charge, rapid
charge is stopped, and the charge method is switched over to
trickle charge.
   Approx. 1 to 2°C/min. When a rise in the
battery temperature per unit time is detected by a thermistor
or other type of temperature sensor during rapid charge, and
the prescribed temperature rise is sensed, rapid charge is
stopped and the charge method is switched over to trickle
charge.
55°C (for A and AA size), 5C
(for AAA size), 6C (for L-A, LfatA and SC size). The cycle
life and other characteristics of batteries are impaired if the
batteries are allowed to become too hot during charge. In
order to safeguard against this, rapid charge is stopped and
the charge method is switched over to trickle charge when
the battery temperature has reached the prescribed level.
to 10 min. This prevents the - ∆V detec-
tion circuit from being activated for a specific period of time
after rapid charge has commenced. However, the dT/dt
detection circuit is allowed to be activated during this time.
As with Ni-Cd batteries, the charge voltage of Ni-MH batteri
es
may show signs of swinging (pseudo - ∆V)
when they have been
kept standing for a long time or when they have discharged
excessively, etc. The initial delay timer is needed to prevent
charge from stopping (to prevent malfunctioning) due to this
pseudo - ∆V.
   0.033 to 0.05CmA. When the trickle
current is set higher, the temperature rise of the batteries is
increased, causing the battery characteristics to deteriorate.
 60 min.
 90 min. (at 1C charge)
   10 to 20 hours. The overcharging of Ni-MH
batteries, even by trickle charging, causes a
deterioration in
the characteristics of the batteries. To prevent
overcharging by
trickle charging or any other charging method, the provision
of
a timer to regulate the total charging time is recommended.
The temperature and voltage of Ni-MH batteries varies
depending on the shape of the battery pack, the number of cells,
the arrangement of the cells and other factors. There fore
1818
1919
 
Panasonic should be consulted for more detailed information
on the referenced charge control values. The charge methods
described previously can be applied also when Ni-MH batteries
are employed in a product, but Panasonic should be consulted
for the control figures and other details.



The optimal charge system for the Ni-MH ’H’’ Series for
back-up power applications is an intermittent timer charge.
An intermittent timer charge improves charge efficiency,
extends battery life (-vs- trickle charge) and reduces electri-
city consumption up to 30% compared to trickle charge*2.
(See diagram) At the beginning of
the charge, an IC timer is started and charging is activated at
a current of 0.1lt until the timer stops and the charge is termi-
nated. When the batteries self discharge down to a set point
(1.3V), the timer charge is re-activated.

Average charge current: 0.1ltA
Re-charge time: 16 hours
Pulse charging can be used

1. Rapid charge current Max. 1CmA to 0.5CmA
2. Rapid charge transition voltage
restoration current
0.2 to 0.3CmA
3. Rapid charge start voltage Approx. 0.8V/cell
4. Charge terminating voltage 1.8V/cell
5. ∆V value 5 to 10mV/cell
6. Battery temperature rising rate
dT/dt value
1 to 2°C/min
7.
Maximum battery temperature
TCO 60°C (for L-A, L-fatA and SC size)
55°C (for A, AA and D size)
50°C (for QA, AAA and prismatic size)
8. Initial -∆V detection disabling
timer 5 to 10 min
9. Trickle current (after rapid charge)
0.033 to 0.05CmA
10. Rapid charge transfer timer 60 min
11. Rapid charge timer 90 min (at 1CmA charge)
12. Total timer 10 to 20 hours
13. Rapid charge temperature range 0° to 40°C
*1 Matching test is required because these values vary depending on rapid charge current, number of cells, configuration of battery pack, etc.
*2 Trickle charge is not recommended in general for Ni-MH batteries. Please consult Panasonic on any Ni-MH applications requiring trickle charge.
4
Fig 1
Battery Voltage
Battery Te mperature
Charge Current
Time
Voltage
Current
Te mp.
1
13
6
7
9
11
12
2
10
3
8
5
Capacity Current Voltage
(mAh) (mA) (V)
7 days
0.1lt*16h 0.1lt*4h0.1lt*4h
7 days
Initial charge Discharge Charge Discharge Charge Discharge
(Self discharge) (Self discharge) (Self discharge)
(Ambient Temp 20°C)
Fig 2
Thermistor
Thermal Protector
T
-
+





Voltage range
_____V max. _____V min.
Load pattern
Continuous load
___________mA (max.)
___________mA (av.)
___________mA (min.)
Intermittent load/pulse load
___________mA (max.)
___________mA (av.)
___________mA (min.)
Intermittent time conditions
Operating time
___________
Stopped time
___________

Rapid charge
Trickle float charge
Charge time
Charge temperature and atmosphere

Temperature and humidity during use
_____°C max._____°C min.
_____% max. _____% min.
Temperature and humidity during
storage
_____°C max._____°C min.
_____% max. _____% min.

Operating life
_____________________
Storage period
_____________________


Diameter (mm)_______max.
Height (mm)_______max.
Length (mm)_______max.
Width (mm)_______max.
Mass (g)__________av.
Terminal type ___________

Atmospheric pressure
Mechanical conditions
Safety
_____________________
Interchangeability
Marketability
Price




Verify the battery specifications required for the power supply
of the device and use those conditions as the standards for
battery selection. For reference, the technological factors
concerning battery selection are shown below.

Using the catalogs and data sheets for the batteries currently
produced and marketed, narrow down the number of
candidates to a few battery types. From those candidates,
select the one battery that most closely satisfies the ideal
conditions required. In actual practice, the selection of a
battery is rarely completed as easily as this. In most cases it
is necessary to consider eliminating or relaxing some of the
proposed specifications, and then select the most suitable
battery from among those currently available to meet the
adjusted conditions. This process makes it possible to select
more economical batteries. If you have any doubts at this
stage, consult closely with a battery engineer. In some cases,
newly improved or newly developed batteries that are not yet
listed in the catalog may be available. Normally the required
specifications are also finalized at this stage.
2020
2121


Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.
 HHR-70AAA/FT
 10.5 +0 / -0.7
 44.5 +0 / -1.0
 12
 1.2

 730
 700

30
  70 x 16
 700 x 1.2

  0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55



 
   

  
  
  
HHR-70AAA/FT AAA AAA 1.2 730 700 10.5 +0/-0.7 44.5 +0/-1.0 12 HR11/45 21
HHR-75AAA/HT*3AAA AAA 1.2 730 700 10.5 +0/-0.7 44.5 +0/-1.0 12 HR11/45 22
HHR-80AAA/HT*3AAA AAA 1.2 780 750 10.5 +0/-0.7 44.5 +0/-1.0 13 HR11/45 23
HHR-35AA/FT AA 2/3AA 1.2 390 350 14.5 +0/-0.7 28.5 +0/-1.0 10.5 - 24
HHR-120AA/FT AA 4/5AA 1.2 1,220 1,150 14.5 +0/-0.7 43.0 +0/-1.0 23 HR15/43 25
HHR-70AA/FT AA AA 1.2 780 700 14.5 +0/-0.7 48.8 +0/-1.5 21 HR15/49 26
HHR-70AA/HT*4AA AA 1.2 780 700 14.5 +0/-0.7 50.5 +0/-1.5 21 HR15/49 27
HHR-110AA/FT AA AA 1.2 1,180 1,100 14.5 +0/-0.7 50.0 +0/-1.0 24 HR15/51 28
HHR-150AA/FT AA AA 1.2 1,580 1,500 14.5 +0/-0.7 50.0 +0/-1.0 26 HR15/51 29
HHR-210AA/HT*4AA AA 1.2 2,080 2,000 14.5 +0/-0.7 50.5 +0/-1.0 29 HR15/51 30
HHR-200A/FT A4/5A 1.2 2,040 2,000 17.0 +0/-0.7 43.0 +0/-1.5 32 HR17/43 31
HHR-210A/FT AA 1.2 2,200 2,100 17.0 +0/-0.7 50.0 +0/-1.5 38 HR17/50 32
HHR-380A/FT AL-A 1.2 3,800 3,700 17.0 +0/-0.7 67.0 +0/-1.5 53 HR17/67 33
HHR-450A/FT ALFat/A 1.2 4,500 4,200 18.2 +0/-0.7 67.0 +0/-1.5 60 - 34
HHR-200SCP/FT*5SC 4/5SC 1.2 2,100 1,900 23.0 +0/-1.0 34.0 +0/-1.5 43 - 35
HHR-260SCP/FT*5SC SC 1.2 2,600 2,450 23.0 +0/-1.0 43.0 +0/-1.5 55 HR23/43 36
HHR-300SCP/FT*5SC SC 1.2 3,050 2,800 23.0 +0/-1.0 43.0 +0/-1.5 57 HR23/43 37
   

  
  
  
HHR-60AAAH/FT AAA AAA 1.2 550 500 10.5 +0/-0.7 44.5 +0/-1.0 13 HR11/45 38
HHR-70AAH/FT AA AA 1.2 750 700 14.5 +0/-0.7 48.3 +0/-1.0 18 HR15/49 39
HHR-210AH/FT A A 1.2 2,050 1,900 17.0 +0/-0.7 50.0 +0/-1.5 36 HR17/50 40
HHR-330APH/FT*5A LFat/A 1.2 3,300 3,200 18.2 +0/-0.7 67.0 +0/-1.5 60 - 41
HHR-370AH/FT A LFat/A 1.2 3,700 3,500 18.2 +0/-0.7 67.0 +0/-1.5 60 - 42
HHR-250SCH/FT*5SC SC 1.2 2,650 2,500 23.0 +0/-1.0 43.0 +0/-1.5 55 HR23/43 43
HHR-300CH/FT*5C C 1.2 3,300 3,100 26.0 +0/-1.0 50.0 +0/-2.0 80 HR26/50 44
  

  
 
   
HHR-9SRE/BA1 E-Block 8.4 175 170 26.0 48.5 16.3 42 -





Cap shape: This appendix is used when there
is a flat top (HT stands for high top battery).
Designed for high ambient temperature
Diameter: AAA, AA, A
Multiply this by 10 to obtain the rated capacity (some exceptions)
Round
Panasonic Nickel-Metal-Hydride battery
*1 After charging at 0.1 CmA for 16 hours, discharging at 0.2 CmA.
*2 For reference only.
*3 Compatible with consumer AAA size.
*4 Compatible with consumer AA size.
*5 For high power use applications such as Powertools.
700mA(1 lt)
1400mA(2 lt)
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
140mA(0.2 lt)
Charge: 700mA(1 lt) x 1.2hrs.
0°C
20°C
40°C
Charge time (minutes)
Discharge time (hours)
0 10 20 30 40 50 60 70 80 90 100
0 1 2 3 4 5 6
Charge: 700mA(1 lt) x 1.2hrs.
2.0
1.9
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
0°C
20°C
40°C
700mA(1 lt)
1400mA(2 lt)
Voltage (V)Voltage (V)Voltage (V)
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
140mA(0.2 lt)
Discharge time (minutes)
0 10 20 30 40 50 60 70 80
700mA(1 lt)
1400mA(2 lt)
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
140mA(0.2 lt)
Charge: 700mA(1 lt) x 1.2hrs.
0°C
20°C
40°C
Charge time (minutes)
Discharge time (hours)
0 10 20 30 40 50 60 70 80 90 100
0 1 2 3 4 5 6
Charge: 700mA(1 lt) x 1.2hrs.
2.0
1.9
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
0°C
20°C
40°C
700mA(1 lt)
1400mA(2 lt)
Voltage (V)Voltage (V)Voltage (V)
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
140mA(0.2 lt)
Discharge time (minutes)
0 10 20 30 40 50 60 70 80
700mA(1 lt)
1400mA(2 lt)
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
140mA(0.2 lt)
Charge: 700mA(1 lt) x 1.2hrs.
0°C
20°C
40°C
Charge time (minutes)
Discharge time (hours)
0 10 20 30 40 50 60 70 80 90 100
0 1 2 3 4 5 6
Charge: 700mA(1 lt) x 1.2hrs.
2.0
1.9
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
0°C
20°C
40°C
700mA(1 lt)
1400mA(2 lt)
Voltage (V)Voltage (V)Voltage (V)
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
Charge: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
140mA(0.2 lt)
Discharge time (minutes)
0 10 20 30 40 50 60 70 80
Ø10.5
0
- 0.7
Ø10.5
0
- 0.7
44.5
0
- 1.0
2222
Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.





2323

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.




C
20°C
40°C
Charge: 450mA(0.64 lt) 1.7hrs.
140mA(0.2 lt)
Charge: 450mA(0.64 lt) 1.7hrs. 20°C
Discharge temperature: 20°C
700mA(1 It)
1400mA(2 It)
Charge
: 450mA(0.64 lt) 1.7hrs. 20°C
Discharge temperature
: 20°C
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
Discharge time (hours)
0 1 2 3 4 5 6
Charge time (minutes)
0 10 20 30 40 50 60 70 80 90 100110 120
2.0
1.9
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
Discharge time (minutes)
0 10 20 30 40 50 60 70 80
C
20°C
40°C
Charge: 450mA(0.64 lt) 1.7hrs.
140mA(0.2 lt)
Charge: 450mA(0.64 lt) 1.7hrs. 20°C
Discharge temperature: 20°C
700mA(1 It)
1400mA(2 It)
Charge
: 450mA(0.64 lt) 1.7hrs. 20°C
Discharge temperature
: 20°C
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
Discharge time (hours)
0 1 2 3 4 5 6
Charge time (minutes)
0 10 20 30 40 50 60 70 80 90 100110 120
2.0
1.9
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
Discharge time (minutes)
0 10 20 30 40 50 60 70 80
0°C
20°C
40°C
Charge: 450mA(0.64 lt) 1.7hrs.
140mA(0.2 lt)
Charge: 450mA(0.64 lt) 1.7hrs. 20°C
Discharge temperature: 20°C
700mA(1 It)
1400mA(2 It)
Charge
: 450mA(0.64 lt) 1.7hrs. 20°C
Discharge temperature
: 20°C
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
Discharge time (hours)
0 1 2 3 4 5 6
Charge time (minutes)
0 10 20 30 40 50 60 70 80 90 100110 120
2.0
1.9
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Voltage (V)
Discharge time (minutes)
0 10 20 30 40 50 60 70 80
 HHR-75AAA/HT
 10.5 +0/-0.7
 44.5 +0/-1.0
 12
 1.2

 730
 700

35
  70 x 16
 450 x 1.7

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55
Ø10.5
0
- 0.7
Ø10.5
Ø3.75
0
- 0.7
0
- 0.7
44.5
0
- 1.0
1.3

0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
1.9
2.0
0 10 20 30 40 50 60 70 80 90 100
0°C
20°C
45°C
Voltage (V)
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
0 1 2 3 4 5 6
Voltage (V)
Discharge time (hours)
150mA(0.2 It)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
0 10 20 30 40 50 60 70 80
750mA(1 It)
1500mA(2 It)
Voltage (V)
Dischar
e time (minutes)
Test condition: (1.0 ltA=750mA)
Charge: 0.1ltA x 16h
Rest: 5h
Discharge: 0.2ltA to 1.0V
Discharge temperature: 20°C
Test condition: (1.0 lt A=750mA)
Charge: 0.1lt A x 16h
Rest: 5h
Discharge: 0.2lt A to 1.0V
Discharge temperature: 20°C
Text condition (1.0 lt=750mA)
Charge: 1.0 lt-5mV
Discharge temperature: 0, 20, 45°C
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
1.9
2.0
0 10 20 30 40 50 60 70 80 90 100
0°C
20°C
45°C
Voltage (V)
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
0 1 2 3 4 5 6
Voltage (V)
Discharge time (hours)
150mA(0.2 It)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
0 10 20 30 40 50 60 70 80
750mA(1 It)
1500mA(2 It)
Voltage (V)
Dischar
e time (minutes)
Test condition: (1.0 ltA=750mA)
Charge: 0.1ltA x 16h
Rest: 5h
Discharge: 0.2ltA to 1.0V
Discharge temperature: 20°C
Test condition: (1.0 lt A=750mA)
Charge: 0.1lt A x 16h
Rest: 5h
Discharge: 0.2lt A to 1.0V
Discharge temperature: 20°C
Text condition (1.0 lt=750mA)
Charge: 1.0 lt-5mV
Discharge temperature: 0, 20, 45°C
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
1.9
2.0
0 10 20 30 40 50 60 70 80 90 100
C
20°C
45°C
Voltage (V)
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
0 1 2 3 4 5 6
Voltage (V)
Discharge time (hours)
150mA(0.2 It)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
0 10 20 30 40 50 60 70 80
750mA(1 It)
1500mA(2 It)
Voltage (V)
Dischar
e time (minutes)
Test condition: (1.0 ltA=750mA)
Charge: 0.1ltA x 16h
Rest: 5h
Discharge: 0.2ltA to 1.0V
Discharge temperature: 20°C
Test condition: (1.0 lt A=750mA)
Charge: 0.1lt A x 16h
Rest: 5h
Discharge: 0.2lt A to 1.0V
Discharge temperature: 20°C
Text condition (1.0 lt=750mA)
Charge: 1.0 lt-5mV
Discharge temperature: 0, 20, 45°C
 HHR-80AAA/HT
 10.5 +0/-0.7
 44.5 +0/-1.0
 13
 1.2

 780
 750

45
  75 x 16
 750 x 1.2

  0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55
Ø10.5
0
- 0.7
Ø10.5
Ø3.6
0
- 0.7
0
- 0.5
44.5
0
- 1.0
0
+1.5
0 min 0.8

2424

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.





2525

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.



Charge time (minutes)
Discharge time (hours)
Dischar
g
e time (minutes)
0 10 20 30 40 50 60 70 80 90 100
0 1 2 3 4 5 6
Charge: 350mA(1.0 lt) x 1.2hrs.
2.0
1.8
1.6
1.4
1.2
1.0
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
0°C
20°C
40°C
Voltage(V)Voltage(V)Voltage(V)
Charge: 350mA(1.0 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
70mA(0.2 lt)
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.0
1.1
0.9
0.8 0 10 20 30 40 50 60 70 80 90 100
Charge: 350mA(1.0 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
350mA(1 lt)
700mA(2 lt)
Charge time (minutes)
Discharge time (hours)
Dischar
g
e time (minutes)
0 10 20 30 40 50 60 70 80 90 100
0 1 2 3 4 5 6
Charge: 350mA(1.0 lt) x 1.2hrs.
2.0
1.8
1.6
1.4
1.2
1.0
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
0°C
20°C
40°C
Voltage(V)Voltage(V)Voltage(V)
Charge: 350mA(1.0 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
70mA(0.2 lt)
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.0
1.1
0.9
0.8 0 10 20 30 40 50 60 70 80 90 100
Charge: 350mA(1.0 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
350mA(1 lt)
700mA(2 lt)
Charge time (minutes)
Discharge time (hours)
Dischar
g
e time (minutes)
0 10 20 30 40 50 60 70 80 90 100
0 1 2 3 4 5 6
Charge: 350mA(1.0 lt) x 1.2hrs.
2.0
1.8
1.6
1.4
1.2
1.0
0.8
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
0°C
20°C
40°C
Voltage(V)Voltage(V)Voltage(V)
Charge: 350mA(1.0 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
70mA(0.2 lt)
1.8
1.7
1.6
1.5
1.4
1.3
1.2
1.0
1.1
0.9
0.8 0 10 20 30 40 50 60 70 80 90 100
Charge: 350mA(1.0 lt) x 1.2hrs. 20°C
Discharge temperature: 20°C
350mA(1 lt)
700mA(2 lt)
Ø14.5
0
- 0.7
28.5
0
- 1.0
 HHR-35AA/FT
 14.5 +0/-0.7
 28.5 +0/-1.0
 10,5
 1.2

 390
 350

30
  35 x 16
 350 x 1.2

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

0°C
20°C
40°C
Charge
: 1200mA(1 lt) x 1.2hrs.
0123456
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
240mA(0.2 lt)
Charge
: 1200mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V) Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.6
1.7
1.8
1200mA(1 lt)
2400mA(2 lt)
Charge
: 1200mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
80 90 1007010 20 30 40 50 600
Charge time (minutes)
807010 20 30 40 50 600
Discharge time (minutes)
Discharge time (hours)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
C
20°C
40°C
Charge
: 1200mA(1 lt) x 1.2hrs.
0123456
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
240mA(0.2 lt)
Charge
: 1200mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V) Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.6
1.7
1.8
1200mA(1 lt)
2400mA(2 lt)
Charge
: 1200mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
80 90 1007010 20 30 40 50 600
Charge time (minutes)
807010 20 30 40 50 600
Discharge time (minutes)
Discharge time (hours)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
C
20°C
40°C
Charge
: 1200mA(1 lt) x 1.2hrs.
0123456
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
240mA(0.2 lt)
Charge
: 1200mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V) Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.6
1.7
1.8
1200mA(1 lt)
2400mA(2 lt)
Charge
: 1200mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
80 90 1007010 20 30 40 50 600
Charge time (minutes)
807010 20 30 40 50 600
Discharge time (minutes)
Discharge time (hours)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
Ø14.5
0
- 0.7
43.0
0
- 1.0
 HHR-120AA/FT
 14.5 +0/-0.7
 43.0 +0/-1.0
 23
 1.2

 1,220
 1,150

19
  120 x 16
 1,200 x 1.2

  0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

2626

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.





2727

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.



C
20°C
40°C
Charge:
700mA(1 lt) x 1.2hrs.
140mA(0.2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
700mA (1 lt)
1400mA (2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
Voltage (V)
1.6
0123456
Discharge time (hours)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
Voltage (V)
807010 20 30 40 50 600
Discharge time (minutes)
C
20°C
40°C
Charge:
700mA(1 lt) x 1.2hrs.
140mA(0.2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
700mA (1 lt)
1400mA (2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
Voltage (V)
1.6
0123456
Discharge time (hours)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
Voltage (V)
807010 20 30 40 50 600
Discharge time (minutes)
C
20°C
40°C
Charge:
700mA(1 lt) x 1.2hrs.
140mA(0.2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
700mA (1 lt)
1400mA (2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
Voltage (V)
1.6
0123456
Discharge time (hours)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
Voltage (V)
807010 20 30 40 50 600
Discharge time (minutes)
 HHR-70AA/FT
 14.5 +0/-0.7
 48.8 +0/-1.5
 21
 1.2

 780
 700

25
  70 x 16
 700 x 1.2

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55
Ø14.5
0
- 0.7
48.8
0
- 1.5

Ø14.5
0
- 0.7
50.5
0
- 1.5
1.5
Ø5
0°C
20°C
40°C
Charge:
700mA(1 lt) x 1.2hrs.
140mA(0.2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
700mA (1 lt)
1400mA (2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge
temperature: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Dischar
g
e time (minutes)
0°C
20°C
40°C
Charge:
700mA(1 lt) x 1.2hrs.
140mA(0.2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
700mA (1 lt)
1400mA (2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge
temperature: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Dischar
g
e time (minutes)
0°C
20°C
40°C
Charge:
700mA(1 lt) x 1.2hrs.
140mA(0.2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
700mA (1 lt)
1400mA (2 lt)
Charge
: 700mA(1 lt) x 1.2hrs. 20°C
Discharge
temperature: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Dischar
g
e time (minutes)
 HHR-70AA/HT
 14.5 +0/-0.7
 50.5 +0/-1.5
 21
 1.2

 780
 700

25
  70 x 16
 700 x 1.2

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

2828

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.





2929

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.



Ø14.5
0
- 0.7
50.0
0
- 1.0
0°C
20°C
40°C
Charge
: 1100mA (1 lt) x 1.2hrs.
220mA(0.2 It)
Charge
: 1100mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1100mA(1 lt)
2200mA(2 lt)
Charge
: 1100mA(1 It) x 1.2hrs. 20°C
Discharge
temperature: 20°C
Voltage (V)
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
0°C
20°C
40°C
Charge
: 1100mA (1 lt) x 1.2hrs.
220mA(0.2 It)
Charge
: 1100mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1100mA(1 lt)
2200mA(2 lt)
Charge
: 1100mA(1 It) x 1.2hrs. 20°C
Discharge
temperature: 20°C
Voltage (V)
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
0°C
20°C
40°C
Charge
: 1100mA (1 lt) x 1.2hrs.
220mA(0.2 It)
Charge
: 1100mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1100mA(1 lt)
2200mA(2 lt)
Charge
: 1100mA(1 It) x 1.2hrs. 20°C
Discharge
temperature: 20°C
Voltage (V)
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
 HHR-110AA/FT
 14.5 +0/-0.7
 50.0 +0/-1.0
 24
 1.2

 1,180
 1,100

16
  110 x 16
 1,100 x 1.2

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

C
20°C
40°C
Charge
: 1500mA(1 lt) x 1.2hrs.
300mA(0.2 lt)
Charge
: 1500mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
1500mA(1 lt)
3000mA(2 lt)
Charge
: 1500mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Dischar
g
e time (minutes)
C
20°C
40°C
Charge
: 1500mA(1 lt) x 1.2hrs.
300mA(0.2 lt)
Charge
: 1500mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
1500mA(1 lt)
3000mA(2 lt)
Charge
: 1500mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Dischar
g
e time (minutes)
C
20°C
40°C
Charge
: 1500mA(1 lt) x 1.2hrs.
300mA(0.2 lt)
Charge
: 1500mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
1500mA(1 lt)
3000mA(2 lt)
Charge
: 1500mA(1 lt) x 1.2hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Dischar
g
e time (minutes)
 HHR-150AA/FT
 14.5 +0/-0.7
 50.5 +0/-1.0
 26
 1.2

 1,580
 1,500

23
  150 x 16
 1,500 x 1.2

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

Ø14.5
0
- 0.7
50.0
0
- 1.0
3030

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.





3131

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.



C
20°C
40°C
Charge
: 1200mA (0.55 It)- dV=10mV
310mA
Charge
: 1200mA x 2hrs. 20°C
Discharge temperature:
20°C
2000mA(1lt)
4000mA(2lt)
Charge
: 1200mA (0.55 It)-dV=10mV 20°C
Discharge temperatures: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 100 110 1207010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
C
20°C
40°C
Charge
: 1200mA (0.55 It)- dV=10mV
310mA
Charge
: 1200mA x 2hrs. 20°C
Discharge temperature:
20°C
2000mA(1lt)
4000mA(2lt)
Charge
: 1200mA (0.55 It)-dV=10mV 20°C
Discharge temperatures: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 100 110 1207010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
0°C
20°C
40°C
Charge
: 1200mA (0.55 It)- dV=10mV
310mA
Charge
: 1200mA x 2hrs. 20°C
Discharge temperature:
20°C
2000mA(1lt)
4000mA(2lt)
Charge
: 1200mA (0.55 It)-dV=10mV 20°C
Discharge temperatures: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 100 110 1207010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
Ø14.5
0
- 0.7
Ø5.5
0
- 0.7
0
- 0.8
50.5
0
- 1.0
min 1.0
 HHR-210AA/HT
 14.5 +0/-0.7
 50.5 +0/-1.0
 29
 1.2

 2,080
 2,000

20
  200 x 16
 1,200 x 2

  0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

40°C
20°C
C
Charge: 1700mA(0.85 lt) x 1.4hrs.
400mA(0.2 lt)
Charge: 1700mA(0.85 lt) x 1.4hrs. 20°C
Discharge temperature: 20°C
2000mA(1 lt)
4000mA(2 lt)
Charge
: 1700mA(0.85 lt) x 1.4hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
40°C
20°C
C
Charge: 1700mA(0.85 lt) x 1.4hrs.
400mA(0.2 lt)
Charge: 1700mA(0.85 lt) x 1.4hrs. 20°C
Discharge temperature: 20°C
2000mA(1 lt)
4000mA(2 lt)
Charge
: 1700mA(0.85 lt) x 1.4hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
40°C
20°C
0°C
Charge: 1700mA(0.85 lt) x 1.4hrs.
400mA(0.2 lt)
Charge: 1700mA(0.85 lt) x 1.4hrs. 20°C
Discharge temperature: 20°C
2000mA(1 lt)
4000mA(2 lt)
Charge
: 1700mA(0.85 lt) x 1.4hrs. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 90 1007010 20 30 40 50 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.6
1.7
1.8
807010 20 30 40 50 600
Discharge time (minutes)
Ø17.0
0
- 0.7
43.0
0
- 1.5
 HHR-200A/FT
 17.0 +0/-0.7
 43.0 +0/-1.5
 32
 1.2

 2,040
 2,000

20
  200 x 16
 1,700 x 1.4

 0 to +45
 0 to +40
 -10 to +65

< -20 to +35
< -20 to +45
< -20 to +55

3232

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.





3333

Battery performance and cycle life are strongly affected by how they are used. In order to maximize battery safety, please consult Panasonic when determining
charge/discharge specs, warning label contents and design. The data in this document are for descriptive purposes only and are not intended to make or imply any
guarantee or warranty.

*
1
After charging at 0.1It for 16 hours, discharging at 0.2It.
*
2
For reference only.
*
3
Need specially designed control system. Please contact Panasonic for details.



Ø17.0
0
- 0.7
67.0
0
- 1.5
40°C
20°C
C
Charge: 2000mA dT/dt=1.0°C/min. 20°C
760mA(0.2lt)
Charge
: 2000mA dT/dt=1.0°C/min. 20°C
Discharge temperature
: 20°C
2000mA(0.54 lt)
3700mA(1 lt)
Charge
: 2000mA dT/dt=1.0°C/min. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 120140 16010020 40 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
80 90 100110 1207010 20 30 40 50 600
Discharge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
40°C
20°C
C
Charge: 2000mA dT/dt=1.0°C/min. 20°C
760mA(0.2lt)
Charge
: 2000mA dT/dt=1.0°C/min. 20°C
Discharge temperature
: 20°C
2000mA(0.54 lt)
3700mA(1 lt)
Charge
: 2000mA dT/dt=1.0°C/min. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 120140 16010020 40 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
0123456
Discharge time (hours)
80 90 100110 1207010 20 30 40 50 600
Discharge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4
1.5
1.7
1.8
1.6
40°C
20°C
0°C
Charge: 2000mA dT/dt=1.0°C/min. 20°C
760mA(0.2lt)
Charge
: 2000mA dT/dt=1.0°C/min. 20°C
Discharge temperature
: 20°C
2000mA(0.54 lt)
3700mA(1 lt)
Charge
: 2000mA dT/dt=1.0°C/min. 20°C
Discharge temperature
: 20°C
Voltage (V)
1.8
1.9
2.0
1.7
1.6
1.5
1.4
1.3
1.2
1.1
1.0
0.9
0.8
80 120140 16010020 40 600
Charge time (minutes)
Voltage (V)
0.8
0.9
1.0
1.1
1.2
1.3
1.4