Semiconductors, Development Tools

Devices that contains multiple elements and can provide many functions. These devices are built with materials that have an electrical conductivity that falls between the conductivity of a conductor and an insulator.

Clock, Timing Clock, Timing Devices that are designed to provide or manipulate periods of time.
View all Clock, Timing
Data Acquisition Data Acquisition Devices designed to convert signals from one style to another.
View all Data Acquisition
Discrete Semiconductors Discrete Semiconductors Devices that contain an individual circuit and provide a single function. These devices are built with materials that have an electrical conductivity that falls between the conductivity of a conductor and an insulator.
View all Discrete Semiconductors
Embedded Embedded Programmable semiconductor devices that are designed to provide specific functions as part of some other equipment.
View all Embedded
Embedded Computers Embedded Computers Devices designed to be provide processing and control of equipment into which they are placed.
View all Embedded Computers
Interface Interface Devices designed to help facilitate communications between external sources and an electronic circuit.
View all Interface
Isolators, Optoisolators, Photocouplers Isolators, Optoisolators, Photocouplers Devices that are used to electronically separate circuits but still allow for signals to be transferred between the circuits.
View all Isolators, Optoisolators, Photocouplers
Linear Linear Devices where the output is linearly (directly) proportional to the input.
View all Linear
Logic Logic Devices that have an output which is based on a logical operation performed on the input.
View all Logic
Memory Memory Devices used for storage of data.
View all Memory
Power Management Power Management Devices that are designed to control current and voltage in order to extend life of a supply, lower operating costs, reduce energy consumed, etc.
View all Power Management
Programmers, Development Systems Programmers, Development Systems Devices that are used to assess the usability of an electronic component within a circuit and devices that can be used to code instructions into electronic components.
View all Programmers, Development Systems
Audio Special Purpose Audio Special Purpose A semiconductor device designed to filter, drive, amplify, convert, interface, etc., audio signals.
View all Audio Special Purpose