Microcontroller Resources
|
Selection of components while in this section is based on peripheral needs or overall functionality. For example, if the design is primarily focused on the Automotive market, then select the tab labeled "Automotive". If connectivity peripherals such as CAN, USB, IrDA, or I²C are the designs priority, then select the tab labeled "Connectivity".

-
Automotive
-
Capacitive Touch
-
Connectivity
-
Energy Harvesting
-
Industrial
-
Motor Control
-
Multimedia
-
Signal
-
Storage
CAN
|
 CAN (controller area network) is a serial communication protocol that is broadcast based. All nodes are available on a common bus with the ability to send and receive messages. CAN was originally designed for the automotive industry but is now used in other markets such as industrial control.
View Related Parts View Related Application Notes View Related PTMs
|
Capacitive Touch
|
 Capacitive touch sensing is a human interface used to replace mechanical buttons, switches, keypads, sliders, and dials by detecting changes in capacitance caused by a human finger. This technology can be hermetically sealed under an overlay and has no moving parts to wear out.
View Related Parts View Related Application Notes View Related PTMs
|
CAN
|
 CAN (controller area network) is a serial communication protocol that is broadcast based. All nodes are available on a common bus with the ability to send and receive messages. CAN was originally designed for the automotive industry but is now used in other markets such as industrial control.
View Related Parts View Related Application Notes View Related PTMs
|
I²C
|
 I²C (Inter-Integrated Circuit) is a communication protocol using two bi-directional lines. These lines are made up of the Serial Data (SDA) and Serial Clock (SCL). This type of communication is used to connect a master to multiple slaves that are uniquely addressed on the bus.
View Related Parts View Related Application Notes View Related PTMs
|
SPI
|
 SPI (serial peripheral interface) is a communication protocol that uses either 3 or 4 wires to transmit data. A master device talks to one or more slaves specifying the slave via a serial clock (SCL), master output/slave input (MOSI), master input/slave output (MISO), and a slave select line.
View Related Parts View Related Application Notes View Related PTMs
|
USB
|
 USB (universal serial bus) is a serial communication standard that is commonly the interface between a computer and peripheral devices. A uniform socket, plug-and-play capability, and power supply for low-power devices makes this protocol flexible. There are multiple versions of USB including 1.0 (full-speed), 2.0 (hi-speed) and OTG (on the go).
View Related Parts View Related Application Notes View Related PTMs
|
Wireless
|
 Wireless communication can provide a simple link between two devices or provide the interface requirements for a complete mesh network with thousands of nodes. Key features of different wireless technologies can include frequency, power usage, and power output. With the broadest selection of wireless devices and components in the industry, Digi-Key can provide you with a complete solution for your wireless design with flexibility in your component decision.
View Wireless Technology Zone
|
Energy Harvesting
|
Energy harvesting is the process by which energy is derived from external sources (e.g. solar power, thermal energy, wind energy, salinity gradients, and kinetic energy), captured, and stored. Frequently the energy is used for small electronic devices such as RF wireless based sensing systems, or where a device is used in a remote location away from a power station.
View Related Parts
|
CAN
|
 CAN (controller area network) is a serial communication protocol that is broadcast based. All nodes are available on a common bus with the ability to send and receive messages. CAN was originally designed for the automotive industry but is now used in other markets such as industrial control.
View Related Parts View Related Application Notes View Related PTMs
|
Brushed DC
|
 BDC (Brushed DC) motors operate directly from DC power sources using an internal commutator, a set of fixed permanent magnets, and a rotating electromagnet armature. Advantages of a brushed DC motor include simple speed control, high reliability, and low cost.
View Related Parts View Related Application Notes View Related PTMs
|
Brushless DC
|
 BLDC (Brushless DC motor) uses a magnet located on the rotor along with fixed magnets on the housing of the motor. The direct current supply is converted into 3 phase alternating current by a device to provide power to the motor. Brushless motors provide an efficient solution with a long life span.
View Related Parts View Related Application Notes View Related PTMs
|
Stepper
|
 A stepper motor is a brushless motor that divides a full revolution into multiple steps. These steps are created for precise movement without the need for feedback. Applications where speed and resolution are critical such as CNC machines, positioning equipment, packing machinery, printers are an ideal fit for these devices.
View Related Parts View Related Application Notes View Related PTMs
|
Display
|
 A display is an output device used to present visual information and to interact with a digital system. Microcontrollers create, manipulate, and interface with a display using an integrated module or an external display controller.
View Related Parts View Related PTMs
|
Signal
|
 ADC (Analog-to-Digital Converter) is an electrical circuit that converts continuous analog signals into discrete digital quantities.
View Related Parts
|
MultiMediaCard
|
 MMC (MultiMediaCard) is a flash memory card standard based on NAND flash memory. MMC cards are used in various portable devices such as multimedia players, digital camcorders, PDAs, and mobile phones.
View Related Parts
|
Secure Digital
|
 SD (Secure Digital) is a non-volatile memory card format jointly developed by Matsushita, SanDisk, and Toshiba. The SD card measures 24mm x 32mm x 2.1mm, has a capacity up to 2 GB and operates on 2.7V - 3.6V.
View Related Parts
|
|
Microcontroller Suppliers - Functional Peripheral
|